"Class C" line harmonic distortion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Class C" line harmonic distortion

706件の閲覧回数
davelove
Contributor I

TEA1716, certain IC production lots have jump instability between 125KHz fixed frequency operational state, and normal fixed Ton state with valley skipping.

This is causing current spike near zero crossing, which is causing Class C line harmonics failure.

How to fix this instability?

0 件の賞賛
1 返信

627件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello David,

Please refer to the attached file. It concerns the TEA1713, but the same method can be used for TEA1716. We do not offer a 380kHz limit version for the TEA1716. So, only the modulation by capacitor to COMPPFC can help to improve.

Best regards,

Tomas

0 件の賞賛