put OM15080-K32W

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

put OM15080-K32W

550 Views
aws1995
Contributor I

Hallo,

i try to use JN51xx Device Programmer to understand how to flash file to usb OM15080-K32W Dongle, and for that i have the two questions :

1) how i can build the the example of sdk of k32 , from MCUXpesso IDE, right ?

then shall use the hex file and flash it to the usb Dongle ?

2) second question i have always this problem when i need to connect to the usb-dongle using serial connection , and i saw , must be set the board into the Programing model , how i can do that ? and ther is some clear to this dongle k32 usb ?

aws1995_0-1629376294877.png

,regards

0 Kudos
Reply
1 Reply

530 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. You need to generate the binary, please refer to section 19.11.1 of the MCUXpresso IDE User Guide.

Can you try with the DK6 Production Flash Programmer (DK6Programmer.exe)? (Path: SDK_K32W061DK6\tools\JN-SW-4407-DK6-Flash-Programmer)

You can follow the instructions of section 1.4 of the DK6 Production Flash Programmer User Guide (Path: SDK_K32W061DK6_doc\docs)

 

Hope this helps. If you have any question let me know.

Best Regards,

Ricardo

0 Kudos
Reply