Hello Gady,
please see below an answer from an application engineer I have contacted.
DESCRIPTION
The problem is that the chip on Device is not working , it don't recognize the Host so I don't have connection of the camera to pc.
[A] Customer will need to change the device board’s PTN5150 PORT pin to pull high (to make if DFP, so it can detect a device plug into the port) – if not possible to change to pull up, then at least leave it as floating (remove the pull down resistor R61 ) , then PTN5150 will work as DRP mode, and still able to detect the camera.
According the datasheet of PTN5150A the pin ADR must be floating or mid so I can use him to be output and get indication if there is connection.
[A] THAT’S correct. Since I don’t see customer use I2C, then they should not pull up or pull down the ADR pin. (and by the way, you can’t pull up R57 to VBUS level. It is not correct)

About the OM13584 I see the schematic as a reference but it's for type-c to type-a, in this case it's work. my problem is the connection of type-c to type-c (host and device has type-c connector and the same chip). pin PORT in host is connected to PULL-DOWN (UFP) and the device the pin PORT is connected to PULL-UP (DFP) and I don't have a connection between him/
[A] I don’t understand this part of the problem. “pin PORT in host is connected to PULL-DOWN (UFP) and the device the pin PORT is connected to PULL-UP (DFP)” -> this is correct.
-> “I don't have a connection between him/” -> not sure what this means here.
With Best Regards,
Jozef