hi
i have centos 6.5(final) on virtual machine and i want to run ltib on it. after running ./install script,when i run ./ltib script, there is following error :
ltib cannot be run because one or more of the host packages needed
to run it are either missing or out of date.
Please install/upgrade these packages and then re-try.
Package Minimum ver Installed info
------- ----------- ---------------
glibc-devel 0 not installed
rpm-build 0 not installed
Died at ./ltib line 1265.
traceback:
main::host_checks:1265
main:479
Started: Tue Jul 28 16:54:39 2015
Ended: Tue Jul 28 16:54:40 2015
Elapsed: 1 seconds
Build Failed
but it seems that i have the packages.when i run yhe following command : sudo yum install glibc-devel ,there is :
Loaded plugins: fastestmirror, refresh-packagekit, security
Setting up Install Process
Loading mirror speeds from cached hostfile
* base: mirror.vit.com.tr
* extras: mirror.vit.com.tr
* rpmforge: mirror.smartmedia.net.id
* updates: mirror.vit.com.tr
Package glibc-devel-2.12-1.149.el6_6.9.x86_64 already installed and latest version
Nothing to do
what is the problem?!
plz help me
thenks
mohammad