pca9634

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pca9634

1,955 Views
marius_haeffner
Contributor I

Hello,

I have a problem with NXP´s LED driver pca9634 and its I2C communication. (datasheet).

For setup and programming I followed the instructions of the datasheet.

SETUP

  • i2c master µC: ATMEGA32U4 (datasheet).
  • The PCA9634 is the only bus slave so i chose the address 0x01 (A0=HIGH and A1..A6 connected to gnd).
  • bus speed: 100kHz
  • pull up resistors: 4k7 (Vdd = 5V)
  • LED resistors 430 ohms / I = 11mA

The schematic is attached.

PROBLEM

The PCA9634 works fine for a while (about 10 minutes) then it stucks at the current state (blinking, permanent on/off).

Analyzing the signals with an oscilloscope shows:

  • SDA = 5V
  • SCL = 1V constant.

After power off/on reset the chip does not work anymore at all!

Furthermore I used another µC as master (SAMat03463 --> datasheet) and in a third scenario an i2c-USB emulator.

I always have the same result as described.

Does anybody has an advice for this issue or had a similar behavior?

I`m very grateful for every response.

Best regards,

Marius

0 Kudos
Reply
4 Replies

1,146 Views
Spiffy_Guy
Contributor I

I also have a problem with PCA9634.  It involves GLOBAL DIMMING.  I am driving a Simple 7 seg LED and I would like all segments at the same brightness I set the Global dimming to 0x7F. MODE1 and MODE2 are 0x00    and I set LEDOUT0  and LEDOUT1 to be my pattern for Each Character.  I wrote a 11 to the Segments I wanted on.   very little OVERHEAD, It should involve writing only three Registers and the LEDOUT can be written one after the other.

 

Again GLOBAL DIMMING may not work, It works fine with LED0 - LED7 Dimming.

 

The Way I am setting the BITS in LEDOUT is to set the Segment I want on to be 1 1.

 

From the Manual, I set LDRx  to allow BOTH CHANNEL DIMMING and GROUP DIMMING

 

When all PWM registers for Each Channel are ZERO and ONLY GRPPWM has a VALUE THE LEDS stay off. 

 

As an experiment, I left GRPPWM at 0x7F and I wrote 0x7F to EVERY PWM0 - PWM7 register and the LEDs work.

 

What I am under the Impression of, that GROUP PWM does not seem to work on this chip.  And because it does not work my debug time was greatly extended.

Spiffy_Guy_0-1708650513043.png

 

0 Kudos
Reply

1,822 Views
marius_haeffner
Contributor I

Hi,

I updated my question and attached the complete schematic

0 Kudos
Reply

1,822 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Marius

Could you please show your complete schematic file of PDF format?

0 Kudos
Reply

1,822 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Can you give the complete schematic for analysis?

0 Kudos
Reply