nvt2006

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

nvt2006

725件の閲覧回数
jean-yves-decos
Contributor I

I have a circuit with the NVT2006BS,188 (joined), trying to shift between VrefA(1.8V) and VrefB(3.3V). With a 20k square signal to test the circuit on An, I have a 1.8V square signal on Bn, even with the 3.3V pull-ups. If I do the opposite, i get 2.37V on An. We added the 200k resistance before EN and VrefB, didn't change the results. Anything you can suggest, we're doing wrong?

タグ(2)
0 件の賞賛
2 返答(返信)

596件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi ,

What do you mean that 'If I do the opposite'?

0 件の賞賛

596件の閲覧回数
jean-yves-decos
Contributor I

Hi,

We resolved it internally, it was an error on our part, thanks anyway!

Jean-yves

De : guoweisun

Envoyé : 16 décembre 2018 21:10

À : Jean-Yves Decoste

Objet : Re: - Re: nvt2006

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: nvt2006

reply from G.w. Sun<https://community.nxp.com/people/guoweisun?et=watches.email.thread> in Other NXP Solutions - View the full discussion<https://community.nxp.com/message/1092237?commentID=1092237&et=watches.email.thread#comment-1092237>

0 件の賞賛