Hello,
I am working on imx93 custom board . where In power on wifi (Murata module ) works fine
mlan0
wfd 0
uap 0
appears properly after scanning
*A TP-Link_5564_5G wifi_a2cdf377f063_54502d4c696e6b5f353536345f3547_managed_psk
*A TP-Link_5564_5G wifi_a2cdf377f163_54502d4c696e6b5f353536345f3547_managed_psk
*A TP-Link_5564_5G wifi_a0cdf377f063_54502d4c696e6b5f353536345f3547_managed_psk
But if i give sw or hw reset then the mlan wifi will not appear after scanning
*A TP-Link_5564_5G wifi_a2cdf377f063_54502d4c696e6b5f353536345f3547_managed_psk
*A TP-Link_5564_5G wifi_a2cdf377f163_54502d4c696e6b5f353536345f3547_managed_psk
Im not getting any solution for this .Kindly help me to get rid of this issue
Regards
Maruti Naik
@Manuel_Salas
Now i have tested in 93 evk L6.1.22 there is no issue
Best Regards !
Maruti Naik
Hello,
As I cannot replicate the issue by my side, could you please share if you are getting kernel logs with dmesg?
If possible, share hardware schematics related to WiFi module.
Best regards,
--... ...--
Salas.
Dear @Manuel_Salas
Thank you for your response.
My issue has been resolved. The problem was caused by the same MAC address being assigned to both mlan0 and wfd0 after resets. By manually changing the MAC address of mlan0, all three networks appeared after scanning.
Best regards!
Maruti Naik
Hello @Maruti
Are you able to test with the i.MX93EVK board? If so, is the issue happening in EVK too?
Best regards,
--... ...--
Salas.