ls1046ardb yocto linux-qoriq config is not getting overwritten by custom kernel config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046ardb yocto linux-qoriq config is not getting overwritten by custom kernel config

Jump to solution
1,554 Views
srechermann
Contributor III

I'm trying to apply some changes to the kernel configuration to my kernel image and to the device tree. In my custom layer my tree looks like this

 

meta-custom/
├── COPYING.MIT
├── README
├── classes
│   └── postprocess_image.bbclass
├── conf
│   └── layer.conf
├── recipes-core
│   └── images
│       └── custom-image.bb
├── recipes-example
│   └── example
│       └── example_0.1.bb
└── recipes-kernel
    └── linux
        ├── linux-qoriq
        │   └── ls1046ardb
        │       ├── 0001-usb0-devicetree-dtsi.patch
        │       └── defconfig
        └── linux-qoriq_5.15.bbappend

 

and thats the content of my linux-qoriq_5.15.bbappend file:

SRC_URI += "file://defconfig"
SRC_URI += "file://0001-usb0-devicetree-dtsi.patch"

FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"

PACKAGE_ARCH = "${MACHINE_ARCH}"

When I'm running `bitbake custom-image` during the build process .patch file is copied to the folder where the linux kernel sources reside (`build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/linux-qoriq`) the devicetree patch get's applied correctly to the .dtsi file (`build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/linux-qoriq/5.15.32+gitAUTOINC+fa6c316859-r0/git/arch/arm64/boot/dts/freescale/fsl-ls1046a.dtsi`) and everything works as expected. But my defconfig file is not getting copied to `build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/linux-qoriq/defconfig` respectively not overwrites the defconfig file that resides in the `build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/linux-qoriq/` folder and is not affecting the `build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/linux-qoriq/build/.conf` file which is used during to kernel build.  What am I doing wrong here?

 

0 Kudos
Reply
1 Solution
1,545 Views
srechermann
Contributor III

Solved the Problem:

I'm now using a config fragment "fragement.cfg" instead of the whole defconfig file.

As described in this post https://community.nxp.com/t5/P-Series/qoriq-Linux-append-the-changes-in-kernel-configuration-not/m-p...  I appended DELTA_KERNEL_DEFCONFIG += "fragment.cfg" to my linux-qoriq_5.15.bbappend file and it looks like this now:

 

SRC_URI += "file://fragment.cfg"
SRC_URI += "file://0001-usb0-devicetree-dtsi.patch"

FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"

DELTA_KERNEL_DEFCONFIG += "fragment.cfg"

PACKAGE_ARCH = "${MACHINE_ARCH}"

 

I have tried using a fragment.cfg file instead of the whole defconfig before but without adding the DELTA_KERNEL_DEFCONFIG += "fragment.cfg" line to my .bbappend file and it did not work.

View solution in original post

0 Kudos
Reply
1 Reply
1,546 Views
srechermann
Contributor III

Solved the Problem:

I'm now using a config fragment "fragement.cfg" instead of the whole defconfig file.

As described in this post https://community.nxp.com/t5/P-Series/qoriq-Linux-append-the-changes-in-kernel-configuration-not/m-p...  I appended DELTA_KERNEL_DEFCONFIG += "fragment.cfg" to my linux-qoriq_5.15.bbappend file and it looks like this now:

 

SRC_URI += "file://fragment.cfg"
SRC_URI += "file://0001-usb0-devicetree-dtsi.patch"

FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"

DELTA_KERNEL_DEFCONFIG += "fragment.cfg"

PACKAGE_ARCH = "${MACHINE_ARCH}"

 

I have tried using a fragment.cfg file instead of the whole defconfig before but without adding the DELTA_KERNEL_DEFCONFIG += "fragment.cfg" line to my .bbappend file and it did not work.

0 Kudos
Reply