LNB for satcom application
1.ku band to L band conversion
2.max. no of I/O channels
NXP offers TFF1044HN that is Ku band down converter for use in LNB of satellite receiver systems. The
device features two RF inputs (two polarizations) and four IF outputs (up to 4 active IF
paths).
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------