This is how I changed the device tree:
&eqos { //no-change-(for a qualcomm based eth chip)
pinctrl-names = "default"; //eth1
pinctrl-0 = <&pinctrl_eqos>;
phy-mode = "rgmii-id";
phy-handle = <ðphy0>;
status = "okay";
mdio {
compatible = "snps,dwmac-mdio";
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
reset-assert-us = <10000>;
reset-gpios = <&gpio4 22 GPIO_ACTIVE_LOW>;
reset-deassert-us = <30000>;
eee-broken-1000t;
at803x,vddio-1p8v;
at803x,vddio-disable;
};
};
};
&fec { //linked to ksz8795
pinctrl-names = "default"; //eth0
pinctrl-0 = <&pinctrl_fec>;
phy-mode = "rgmii-id";
fsl,magic-packet;
status = "okay";
fixed-link {
speed = <1000>;
full-duplex;
};
};
-----------------------------------------------------------------------------------------
&ecspi2 {
#address-cells = <1>;
#size-cells = <0>;
fsl,spi-num-chipselects = <3>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi2 &pinctrl_ecspi2_cs>;
cs-gpios = <&gpio5 13 GPIO_ACTIVE_LOW>, /*SS0*/
<&gpio4 4 GPIO_ACTIVE_LOW>, /*SS1*/
<&gpio4 5 GPIO_ACTIVE_LOW>; /*SS2*/
clocks = <&clk IMX8MP_CLK_ECSPI2_ROOT>,
<&clk IMX8MP_CLK_ECSPI2_ROOT>;
clock-names = "ipg", "per";
status = "okay";
ksz8795: switch@0 {
reg = <0>;
compatible = "microchip,ksz8795";
spi-max-frequency = <5000000>;
pinctrl-names = "default";
/* spi-cpha;
spi-cpol; */
status = "okay";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
label = "lan1";
phy-mode = "rgmii-id";
fixed-link {
speed = <100>;
full-duplex;
};
};
port@1 {
reg = <1>;
label = "lan2";
phy-mode = "rgmii-id";
fixed-link {
speed = <100>;
full-duplex;
};
};
port@2 {
reg = <2>;
label = "lan3";
phy-mode = "rgmii-id";
fixed-link {
speed = <100>;
full-duplex;
};
};
port@4 {
reg = <3>;
label = "cpu";
phy-mode = "rgmii-id";
ethernet = <&fec>;
fixed-link {
speed = <1000>;
full-duplex;
};
};
};
};
spidev1: spi@1 {
reg = <1>;
compatible = "rohm,dh2228fv";
spi-max-frequency = <500000>;
};
spidev2: spi@2 {
reg = <2>;
compatible = "rohm,dh2228fv";
spi-max-frequency = <500000>;
};
};
----------------------------------------------------------------------------
The board is booted and i loads the module: ksz_common, ksz8795 and ksz8795_spi
I can see the respective nodes formed.
# ifconfig
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1501
inet6 fe80::8bd8:a721:8c85:3a61 prefixlen 64 scopeid 0x20<link>
ether 38:d5:47:00:2e:9d txqueuelen 1000 (Ethernet)
RX packets 42 bytes 3094 (3.0 KB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 73 bytes 12753 (12.7 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
eth1: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 38:d5:47:00:2e:9e txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 52
lan1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet6 fe80::f4f3:314b:f7c3:9bd5 prefixlen 64 scopeid 0x20<link>
ether 38:d5:47:00:2e:9d txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 14 bytes 2434 (2.4 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lan2: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet6 fe80::1bd1:9463:93c0:732c prefixlen 64 scopeid 0x20<link>
ether 38:d5:47:00:2e:9d txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 14 bytes 2434 (2.4 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lan3: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet6 fe80::833e:9b97:6b1e:82ae prefixlen 64 scopeid 0x20<link>
ether 38:d5:47:00:2e:9d txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 14 bytes 2434 (2.4 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
-----------------------------------------------------------------------------------------------------------------------------
I can also see an error from the spi-driver
from dmesg log:
DBUG: KSZ_common:ksz_switch_register: of_get_phy_mode returned -22
[ 57.561350] DBUG: KSZ_common:ksz_switch_register: Retrieved PHY mode 0
[ 57.561353] DBUG: KSZ_common:ksz_switch_register: Failed to retrieve PHY mode, error -22
from ksz_common.c:
if (dev->dev->of_node) {
printk("DBUG: KSZ_common:ksz_switch_register: Device tree node found, retrieving PHY mode\n");
ret = of_get_phy_mode(dev->dev->of_node, &interface);
if (ret == 0) {
dev->compat_interface = interface;
printk("DBUG: KSZ_common:ksz_switch_register: Retrieved PHY mode %d\n", interface);
} else {
printk("DBUG: KSZ_common:ksz_switch_register: Failed to retrieve PHY mode, error %d\n", ret);
}
PRINT was added by me to debug-this is the only "error msg" i see from driver. But the driver loads successsfully
Regarding phy-mode: There are other prints after above error :
[ 57.576542] CLSU:KSZ8795: Configuring addr 0x87, bits 0x8, set 1
[ 57.576597] CLSU:KSZ8795: Configuring port 4, offset 0x0, bits 0x40, set 0
[ 57.576631] CLSU:KSZ8795: Configuring port 4, offset 0x2, bits 0x80, set 0
[ 57.576665] CLSU:KSZ8795: Configuring port 4, offset 0x0, bits 0x20, set 1
[ 57.576717] CLSU:KSZ8795: Configuring CPU port
[ 57.576750] CLSU:KSZ8795: Setting RGMII mode
So i suppose the phy-mode is being set to rgmii
----------------------------------------------------------------------------------------------------------------------------------
-------------------------------------------------------------------------------------------------------------------
ISSUE : I connected an ethernet cable between my pc and the board to check the comm ,Set a static ip for eth0 on board. i can see a link is established b/w them . But i cannot ping each other. Data packets are not seem to be receiving at both ends.(Validated that hardware is working fine)
from device to pc
# ping 192.168.1.50
PING 192.168.1.50 (192.168.1.50) 56(84) bytes of data.
From 192.168.1.30 icmp_seq=1 Destination Host Unreachable
Since link is being establish and ping is not happening i suspect - it must be some configuration issue. Either in the device tree or in the Register Writes.
Please help me to troubleshoot the issue.
Solved! Go to Solution.
It worked. The issue was that the driver I used was not updated. It was a 5 port switch. And the fifth port was not registering as it does (N-1) check on the ports. with tot no. of ports set to N=5. Adjusting the value slightly solved the issue.
It worked. The issue was that the driver I used was not updated. It was a 5 port switch. And the fifth port was not registering as it does (N-1) check on the ports. with tot no. of ports set to N=5. Adjusting the value slightly solved the issue.
Hi
You can refer other dts to set switch node.
switch: switch@5f {
compatible = "microchip,ksz9897";
reg = <0x5f>;
pinctrl-0 = <&pinctrl_ksz>;
interrupt-parent = <&gpio4>;
interrupts = <18 IRQ_TYPE_EDGE_FALLING>;
phy-mode = "rgmii-id";
ports {
#address-cells = <1>;
#size-cells = <0>;
lan1: port@0 {
reg = <0>;
label = "lan1";
phy-mode = "internal";
local-mac-address = [00 00 00 00 00 00];
};
lan2: port@1 {
reg = <1>;
label = "lan2";
phy-mode = "internal";
local-mac-address = [00 00 00 00 00 00];
};
lan3: port@2 {
reg = <2>;
label = "lan3";
phy-mode = "internal";
local-mac-address = [00 00 00 00 00 00];
};
lan4: port@3 {
reg = <3>;
label = "lan4";
phy-mode = "internal";
local-mac-address = [00 00 00 00 00 00];
};
port@5 {
reg = <5>;
label = "cpu";
ethernet = <&fec1>;
phy-mode = "rgmii-id";
fixed-link {
speed = <1000>;
full-duplex;
};
};
Best Regards
Zhiming
kernel is 5.10