iMXRT1050 QSPI flash and SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1050 QSPI flash and SDRAM

271 Views
szyba
Contributor I

Hi All, 

iMXRT1050 has dual channel Quad SPI. 

My question is - can I connect to first channel QSPI flash and to second channel QSPI SDRAM??

Can I work with them completely separately and parallel?

Thank you in advance.

Michal

0 Kudos
Reply
1 Reply

243 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello, I hope you are well. 

Yes, FlexSPI has two interfaces so you can connect one memory to each interface.
There are limitations, since they are on the same controller you need to access them separately, if using QSPI as XIP you can have issues while accessing the other memory.

Best regards,
Omar

0 Kudos
Reply