iMX6QP what Vivante driver is necessary for kernel 5.4.24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6QP what Vivante driver is necessary for kernel 5.4.24

2,178 Views
MikeEngel
Contributor IV

Hi all,

we are porting our hardware to the latest NXP BSP and kernel. We have some issues with the Vivante driver support in the new kernel 5.4.24. 

In the past we enabled the CONFIG_DRM_VIVANTE driver and for the the new kernel we have enabled CONFIG_DRM_ETNAVIV. But this driver is not loaded in our kernel. 

Are their any specific configurations necessary to enable that driver?

What driver does NXP use for the iMX6QP and the kernel 5.4.24?

Thanks for your help.

Best regards,

--

Mike

0 Kudos
Reply
2 Replies

2,024 Views
ogj
Contributor IV

Where is the driver imx-gpu-viv-6.2.4.p4.0-aarch32 located? Is it OS agnostic? What is the API for it? Which GPUs does it work with? Any documentation?

0 Kudos
Reply

2,174 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Mike,

 

The vivante driver for MX6 is imx-gpu-viv-6.2.4.p4.0-aarch32 for the MX6 and imx-gpu-viv-6.2.4.p4.0-aarch32 is for the G2D of MX6. but these driver are in binary form and can not be changed. and those CONFIG_DRM_VIVANTE are for MX8.

Regards

 

 

 

0 Kudos
Reply