iMX6QP what Vivante driver is necessary for kernel 5.4.24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6QP what Vivante driver is necessary for kernel 5.4.24

2,165件の閲覧回数
MikeEngel
Contributor IV

Hi all,

we are porting our hardware to the latest NXP BSP and kernel. We have some issues with the Vivante driver support in the new kernel 5.4.24. 

In the past we enabled the CONFIG_DRM_VIVANTE driver and for the the new kernel we have enabled CONFIG_DRM_ETNAVIV. But this driver is not loaded in our kernel. 

Are their any specific configurations necessary to enable that driver?

What driver does NXP use for the iMX6QP and the kernel 5.4.24?

Thanks for your help.

Best regards,

--

Mike

0 件の賞賛
返信
2 返答(返信)

2,011件の閲覧回数
ogj
Contributor IV

Where is the driver imx-gpu-viv-6.2.4.p4.0-aarch32 located? Is it OS agnostic? What is the API for it? Which GPUs does it work with? Any documentation?

0 件の賞賛
返信

2,161件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Mike,

 

The vivante driver for MX6 is imx-gpu-viv-6.2.4.p4.0-aarch32 for the MX6 and imx-gpu-viv-6.2.4.p4.0-aarch32 is for the G2D of MX6. but these driver are in binary form and can not be changed. and those CONFIG_DRM_VIVANTE are for MX8.

Regards

 

 

 

0 件の賞賛
返信