i.MX8M MINI Lop-Power Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M MINI Lop-Power Mode

Jump to solution
1,208 Views
ArtemPN
Contributor I

Hello! 

I`m new to NXP Application processors. I`m working with iMX8M Mini EVK board. I need to bring processor to low-power mode by external event and wake up it also by external event (GPIO lines usage is preferable ). I would like to ask where can I read about procedures of bringing to and waking up from low-power modes for MIMX8MM in details? What can be used as external event source to wake up from low-power mode A53 and M4? Can GPIO lines be controlled by M4 core? 

Thanks in advance!

Artem

0 Kudos
1 Solution
1,191 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
2 Replies
1,181 Views
ArtemPN
Contributor I

Thank you, igor! 

Artem

0 Kudos
1,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi Artem

 

one can look at AN12410

i.MX 8M Mini Power Consumption Measurement

sect.5.2.4.2 Low power mode 

i.MX 8M Mini Applications Processor Reference Manual 

sect.3.1.6 Power modes i.MX 8M Mini Applications Processor Datasheet for Consumer Products

 

Best regards
igor

0 Kudos