Hi Folks,
I have got I.MK8Mq EVK and below are my related queries,
1) Is dual display configuration is possible for HDMI and MX8-DSI-OLED display. As I found that it uses the fsl-imx8mq-evk-dcss-rm67191.dts, which disable the hdmi output by default. If its possible, you please provide steps or patch.
2) Unable to up bluetooth and wifi module. Loading wifi module gives following error message.
root@imx8mqevk:~# [ 363.614928] INFO: task systemd-udevd:2407 blocked for more than 120 seconds.
[ 363.622001] Tainted: G O 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d #1
[ 363.629703] "echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.
[ 363.637652] systemd-udevd D 0 2407 1727 0x0000020d
[ 363.643276] Call trace:
[ 363.645736] [<ffff000008085e98>] __switch_to+0x90/0xc0
[ 363.651001] [<ffff000008c653f0>] __schedule+0x178/0x590
[ 363.656349] [<ffff000008c65844>] schedule+0x3c/0xa8
[ 363.661349] [<ffff000008c688e4>] schedule_timeout+0x174/0x248
[ 363.667414] [<ffff000008c67680>] __down+0x58/0x90
[ 363.672234] [<ffff000008102e74>] down+0x4c/0x68
[ 363.677574] [<ffff000000f4155c>] HIFExchangeBMIMsg+0x20c/0x330 [wlan]
[ 363.684774] [<ffff000000f47ac4>] bmi_download_firmware+0x64/0x130 [wlan]
[ 363.692207] [<ffff000000edff9c>] vos_open+0x174/0x6c0 [wlan]
[ 363.698572] [<ffff000000d9bca4>] hdd_wlan_startup+0x5ac/0x12e0 [wlan]
[ 363.705740] [<ffff000000f45cc8>] hif_pci_probe+0x5f8/0x858 [wlan]
[ 363.711956] [<ffff000008486c4c>] pci_device_probe+0x9c/0x140
[ 363.717734] [<ffff000008649a40>] driver_probe_device+0x1d0/0x2c8
[ 363.723852] [<ffff000008649bf4>] __driver_attach+0xbc/0xc0
[ 363.729532] [<ffff000008647b34>] bus_for_each_dev+0x4c/0x98
[ 363.735223] [<ffff0000086493b8>] driver_attach+0x20/0x28
[ 363.740648] [<ffff000008648fa8>] bus_add_driver+0x1b8/0x228
[ 363.746334] [<ffff00000864a578>] driver_register+0x60/0xf8
[ 363.751933] [<ffff0000084857a8>] __pci_register_driver+0x38/0x40
[ 363.758669] [<ffff000000f45630>] hif_register_driver+0x18/0x38 [wlan]
[ 363.765822] [<ffff000000d93d80>] hdd_hif_register_driver+0x30/0x78 [wlan]
[ 363.773334] [<ffff0000011fa0b4>] hdd_module_init+0xb4/0x1000 [wlan]
[ 363.779722] [<ffff000008083a50>] do_one_initcall+0x38/0x130
[ 363.785411] [<ffff0000081767d8>] do_init_module+0x5c/0x1bc
[ 363.791088] [<ffff000008139650>] load_module+0x1c50/0x20f8
[ 363.796688] [<ffff000008139d78>] SyS_finit_module+0xa8/0xc0
[ 363.802378] [<ffff0000080838d8>] __sys_trace_return+0x0/0x4
3) With Bluetooth I'm getting below logs in dmesg
[ 3.184993] Bluetooth: RFCOMM TTY layer initialized
[ 3.189898] Bluetooth: RFCOMM socket layer initialized
[ 3.195111] Bluetooth: RFCOMM ver 1.11
[ 3.198877] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.204429] Bluetooth: BNEP filters: protocol multicast
[ 3.209694] Bluetooth: BNEP socket layer initialized
[ 3.214804] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.220776] Bluetooth: HIDP socket layer initialized
Then from terminal i executed below commands
root@imx8mqevk:~# systemctl start bluetooth.service
root@imx8mqevk:~# bluetoothctl
Agent registered
[bluetooth]# power on
No default controller available
Found imx6ul board with Murata wifi/bt dev kits for NXP imx. post but not able to map with i.MX8 Mq EVK
Kernel version : NXP i.MX Release Distro 4.9.88-2.0.0 (rocko)
Your suggestions are greatly appreciated. Thank You
Regards,
Rutvij Trivedi.