how to understand the content of s2p file(MRFE6VS25N)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to understand the content of s2p file(MRFE6VS25N)

2,145 Views
530586517
Contributor I

the LDMOS MRFE6VS25N, in the datasheet,at 1030MHz,G=22.5dB;but in it's s2p file , at 1030MHz, S21=2.5917, s21 is not equal to G ……how to understand ?

Labels (1)
  • RF

3 Replies

1,974 Views
LPP
NXP Employee
NXP Employee

1.
S2P header describes conditions used to measure S-parameters

! MRFE6VS25NR1 S-Parameters

! Vdd = 50 Vdc, Idq = 150 mA

# hz S ma R 6.8

S2P data was measured at 6.8 Ohm reference source and load impedances. Please note that 6.8 Ohm impedance is not a matched source/load impedance. Thus, S21 is less than a gain in a matched design.

S2P can be used to calculate MAG (maximum stable gain) and MSG (maximum stable gain).
https://www.microwaves101.com/encyclopedias/stability-factor

2.
The datasheet provides Gps power gain value as measured in NXP 1030 MHz narrowband test circuit.

Please note that datasheet Gps is not a small-signal gain. Gps has been measured at specified high power level. Large signal gain is not equal to those gain values which can be calculated from S-parameters.

You can find more information about the topic:
https://www.nxp.com/docs/en/application-note/AN1526.pdf


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,974 Views
530586517
Contributor I

Dear sir or ma'am,thanks for your suggestions. May i have you attention for three questions?

On the page 23/24 of the datasheet of MRFE6VS25N,there is a reference circuit component layout which contains some kinds of microstrip at 1030MHz.

In conditions of input and output impedance matching via changing values or locations of capacitors or inductors ,can I decrease the width or length of microstrips ? eg. Z6、Z7 and Z11 ....

For narrowband or single frequency application,the impedance matching can be realized easily with less components. Is that right?

At the bottom of the reference circuit component layout,there are some microstrips with nothing components on both sides of cut out area. What is the functions of them?

Look forward to your reply,thank you !

0 Kudos
Reply

1,974 Views
LPP
NXP Employee
NXP Employee

>can I decrease the width or length of microstrips ?

 

Microstrips are parts of the impedance matching network. Changing the width or length of microstrips would require modification of other components (values or locations of capacitors or inductors). Full redesign of the circuits will be needed.

 

>For narrowband or single frequency application,the impedance matching can be realized easily with less components.

 

Indeed. Narrowband design can be implemented with less components.

 

>At the bottom of the reference circuit component layout...

 

These areas are provided for optional gate and drain bias circuit design. The main difference is that the connection points are located closer to the  transistor pads.
Have a great day,

Pavel
TIC

0 Kudos
Reply