Hello All
I have purchased FRDM33771CSPEVB ( IC is MC33771C) development board for battery Management system.
I want to do testing of a battery, Please can anyone help me out how to start with this board
I also have S32K144EVB platform board.
Thanks-
Deepak
已解决! 转到解答。
Hello,
1. Could you please confirm that the hardware is configured as the image below?
2. Have you download and installed the MC33771C/MC33772C (Battery Cell Controller) Evaluation GUI?
Once installed, please go to Info and click on Help. You will be able to review all the steps to run the demo.
I hope this information helps.
Regards,
David
Hello Deepak,
I hope all is great with you.
First, I would like to recommend downloading the User Manual (UM11402) from here. Please review the chapter 3.
Do you have the BATT-14CEMULATOR?
The BATT-14CEMULATOR is a 14-cell battery emulator board that provides an intuitive way to change the voltage across any of the 14 cells and four voltage outputs in order to emulate four external NTC. A minimum of 7 cells and a maximum of 14 cells can be monitored.
Regards,
David
Hello,
1. Could you please confirm that the hardware is configured as the image below?
2. Have you download and installed the MC33771C/MC33772C (Battery Cell Controller) Evaluation GUI?
Once installed, please go to Info and click on Help. You will be able to review all the steps to run the demo.
I hope this information helps.
Regards,
David