I use mpc8313erdb to control nand as data nand and hope to use is as harddisk.
and do as follows I can't get what I want.
can anyone give some help to resolve this.
thank you!
nand flash is K9F5608U0D,
I put the uboot,rootfs(ext2.gz.uboot),kernel ,dtb on the nor flash,
first I write a file to the nand by mtd_debug tool,and can read it back correctly
~ # ./mtd_debug write /dev/mtdblock5 0x40000 502388 aa.txt
~ # ./mtd_debug read /dev/mtdblock5 0x4000 0x09 bb
after I reboot the system it still works well,
but after I poweroff and repower on it goes wrong.
~ # ./mtd_debug read /dev/mtdblock5 0x40000 0x09 bb
end_request: I/O error, dev mtdblock5, sector 0
Buffer I/O error on device mtdblock5, logical block 0
end_request: I/O error, dev mtdblock5, sector 0
Buffer I/O error on device mtdblock5, logical block 0
flash_to_file: read, size 0x9, n 0x9
read(): Input/output error
~ # ./mkfs.jffs2 -o /dev/mtdblock5 -n -b -e 0x4000
end_request: I/O error, dev mtdblock5, sector 0
mkfs.jffs2: write: Input/output error
boot log as follow:
U-Boot 1.3.0 (Jun 9 2015 - 16:10:09) MPC83XX
Reset Status: Software Hard, External/Internal Soft, External/Internal Hard
CPU: e300c3, MPC8313E, Rev: 21 at 333.333 MHz, CSB: 166 MHz
Board: Freescale MPC8313ERDB
I2C: ready
DRAM: 128 MB
FLASH: 16 MB
cpu_init_r () finished
malloc_bin_reloc () finished
NAND: in board_nand_init()
nand maf_id:ec, dev_id:75
mtd->name NAND 32MiB 3,3V 8-bit
nand_flash_ids[i].chipsize 32
in fcm_scan_bbt()
32 MiB
env_relocate () finished
getenv(ethaddr)
getenv_IPaddr
leave pci_init
in devices_init ()
devices_init () finished
jumptable_init () finished
In: serial
Out: serial
Err: serial
Net: TSEC0, TSEC1 [PRIME]
Hit any key to stop autoboot: 0
## Booting image at fe100000 ...
Image Name: Linux-2.6.23
Created: 2015-06-20 6:13:11 UTC
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 1534735 Bytes = 1.5 MB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
## Loading RAMDisk Image at fe400000 ...
Image Name: uboot ext2 ramdisk rootfs
Created: 2015-06-08 12:18:26 UTC
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 5877640 Bytes = 5.6 MB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Booting using the fdt at 0xfec00000
Loading Ramdisk to 0795a000, end 07ef4f88 ... OK
Loading Device Tree to 007fc000, end 007fefff ... OK
Using MPC8313 RDB machine description
Linux version 2.6.23 (gcc version 4.1.2) #425 Sat Jun 20 14:13:10 CST 2015
Found initrd at 0xc795a000:0xc7ef4f88
console [udbg0] enabled
setup_arch: bootmem
mpc8313_rdb_setup_arch()
arch: exit
Zone PFN ranges:
DMA 0 -> 32768
Normal 32768 -> 32768
Movable zone start PFN for each node
early_node_map[1] active PFN ranges
0: 0 -> 32768
Built 1 zonelists in Zone order. Total pages: 32512
Kernel command line:
IPIC (128 IRQ sources) at fdffc700
PID hash table entries: 512 (order: 9, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120756k/131072k available (2812k kernel code, 10156k reserved, 340k data, 95k bss, 136k init)
Mount-cache hash table entries: 512
NET: Registered protocol family 16
Generic PHY: Registered new driver
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
checking if image is initramfs...it isn't (no cpio magic); looks like an initrd
Freeing initrd memory: 5739k freed
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler deadline registered
io scheduler cfq registered
Serial: 8250/16550 driver $Revision: 1.90 $ 4 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0xe0004500 (irq = 18) is a 16550A
serial8250.0: ttyS1 at MMIO 0xe0004600 (irq = 19) is a 16550A
console handover: boot [udbg0] -> real [ttyS1]
RAMDISK driver initialized: 16 RAM disks of 32768K size 1024 blocksize
loop: module loaded
fsl-gianfar fsl-gianfar.0: enabling Lossless Flow Control
eth0: Gianfar Ethernet Controller Version 1.3-skbr, 00:e0:0c:00:95:03
GFAR: SKB Handler initialized at CPU#0(max=32)
eth0: MTU = 1500 (frame size=1526, truesize=1800)
eth0: Running with NAPI enabled
eth0: 64/64 RX/TX BD ring size
Marvell 88E1101: Registered new driver
Marvell 88E1112: Registered new driver
Marvell 88E1111: Registered new driver
Marvell 88E1145: Registered new driver
Fixed MDIO Bus: probed
nor: Found 1 x16 devices at 0x0 in 16-bit bank
Amd/Fujitsu Extended Query Table at 0x0040
nor: CFI does not contain boot bank location. Assuming top.
number of CFI chips: 1
cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.
RedBoot partition parsing not available
physmap-flash nor: Using OF partition information
Creating 5 MTD partitions on "nor":
0x00000000-0x00100000 : "U-Boot"
add_mtd_partitions slave->offset:0
add_mtd_partitions master->size: 16777216
0x00100000-0x00400000 : "Kernel"
add_mtd_partitions slave->offset:1048576
add_mtd_partitions master->size: 16777216
0x00400000-0x00c00000 : "rootfs"
add_mtd_partitions slave->offset:4194304
add_mtd_partitions master->size: 16777216
0x00c00000-0x00c10000 : "DTB"
add_mtd_partitions slave->offset:12582912
add_mtd_partitions master->size: 16777216
0x00c10000-0x00d00000 : "config"
add_mtd_partitions slave->offset:12648448
add_mtd_partitions master->size: 16777216
mtd: partition "config" doesn't start on an erase block boundary -- force read-only
Freescale eLBC NAND Driver (C) 2006-2007 Freescale
nand_get_flash_type type->chipsize: 32
nand_get_flash_type chip->chipsize: 33554432
nand_get_flash_type mtd->erasesize:16384
nand_get_flash_type mtd->writesize:512
nand_get_flash_type mtd->oobsize:16
nand_get_flash_type busw: 0 chip->options:256
nand_get_flash_type chip->badblockpos:5
NAND device: Manufacturer ID: 0xec, Chip ID: 0x75 (Samsung NAND 32MiB 3,3V 8-bit)
nand_scan_ident chip->numchips :1 chip->chipsize: 33554432
nand_scan_tail chip->ecc.steps:1
nand_scan_tail chip->ecc.size:512
nand_scan_tail mtd->writesize:512
nand_scan_bbt bd->options:16384
nand_memory_bbt bd->options:16384
create_bbt Scanning device for bad blocks
create_bbt bd->options 16384,chip 16384
fsl-elbc fsl-elbc.0: Using OF partition information
Creating 1 MTD partitions on "nand":
0x00000000-0x2000000 : "DATA-NAND"
add_mtd_partitions slave->offset:0
add_mtd_partitions master->size: 33554432
mpc83xx_spi.0: MPC83xx SPI Controller driver at 0xc9062000 (irq = 20)
usbmon: debugfs is not available
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
i2c /dev entries driver
rtc-ds1307: probe of 0-0068 failed with error -5
mmc_spi spi28672.0: SD/MMC host mmc0, no DMA, no WP, no poweroff
TCP cubic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
RAMDISK: Compressed image found at block 0
VFS: Mounted root (ext2 filesystem) readonly.
Freeing unused kernel memory: 136k init
mmc0: error -22 whilst initialising SD card
Mounting filesystems
Running sysctl
Setting up networking on loopback device:
Setting up networking on eth0:
Adding static route for default gateway to 192.168.0.1:
Setting nameserver to 192.168.0.1 in /etc/resolv.conf:
Setting up networking on eth1:
SIOCSIFADDR: No such device
eth1: unknown interface: No such device
SIOCSIFNETMASK: No such device
Adding static route for default gateway to 192.168.0.1:
SIOCADDRT: No such device
Setting nameserver to 192.168.0.1 in /etc/resolv.conf:
Starting inetd:
Welcome to Freescale Semiconductor Embedded Linux Environment
!!!!! WARNING !!!!!!!
The default password for the root account is: root
please change this password using the 'passwd' command
and then edit this message (/etc/issue) to remove this message
~ # ls
mkfs.jffs2 mtd_debug openswan
~ # cat /proc/mtd
dev: size erasesize name
mtd0: 00100000 00020000 "U-Boot"
mtd1: 00300000 00020000 "Kernel"
mtd2: 00800000 00020000 "rootfs"
mtd3: 00010000 00020000 "DTB"
mtd4: 000f0000 00020000 "config"
mtd5: 02000000 00004000 "DATA-NAND"
~ # ./mkfs.jffs2 -o /dev/mtdblock5 -n -b -e 0x4000
end_request: I/O error, dev mtdblock5, sector 0
mkfs.jffs2: write: Input/output error
~ # ./mtd_debug read /dev/mtdblock5 0x00 0x09 aa
end_request: I/O error, dev mtdblock5, sector 0
Buffer I/O error on device mtdblock5, logical block 0
end_request: I/O error, dev mtdblock5, sector 0
Buffer I/O error on device mtdblock5, logical block 0
flash_to_file: read, size 0x9, n 0x9
read(): Input/output error
~ #
消息编辑者为:ye yue