how to disable multiples keyboards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to disable multiples keyboards

557件の閲覧回数
sana
Contributor II

Hi team,
currently i am building screens using lvgl gui guider 1.9.1 for our LCD display
In one of my screens i have used 12 texareas where i need to give user input fields hence multiple keybiards are being used how do i disable those i jus need one keyboard for all the textareas.
Basically user needs to give user inputs for multiple fields for this i am using textareas and clicking on tickmark of keyboard triggers a callback to set this is my use case.
Please provide me the solution ASAP.

Thanks and regards,
sahana

0 件の賞賛
返信
4 返答(返信)

424件の閲覧回数
sana
Contributor II

Hi anything on this?
Can the team help me with the faster response.
Thanks and regards,

sahana

0 件の賞賛
返信

530件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

 

  • Create onelv_keyboard for the screen, hide it by default, and reuse it for every text area.
  • On text area focus/click, call lv_keyboard_set_textarea(kb, ta) and show the keyboard.
  • When the user presses OK (✓) on the keyboard, LVGL sends LV_EVENT_READY to the assigned text area—handle that event to commit the value and hide the keyboard.
  • In LVGL v8/v9, adding your own keyboard event handler does not remove the default handler, so you can add callbacks safely
#include "lvgl.h"

static lv_obj_t *kb;

static void ta_focus_cb(lv_event_t *e)
{
    lv_event_code_t code = lv_event_get_code(e);
    lv_obj_t *ta = lv_event_get_target(e);

    if(code == LV_EVENT_FOCUSED || code == LV_EVENT_CLICKED) {
        lv_keyboard_set_textarea(kb, ta);
        lv_obj_clear_flag(kb, LV_OBJ_FLAG_HIDDEN);
    }
}

static void ta_done_cb(lv_event_t *e)
{
    lv_event_code_t code = lv_event_get_code(e);
    lv_obj_t *ta = lv_event_get_target(e);

    if(code == LV_EVENT_READY) {
        const char *val = lv_textarea_get_text(ta);
        /* your commit callback here with `val` */
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
    } else if(code == LV_EVENT_CANCEL) {
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
    }
}

void screen_init(lv_obj_t *parent)
{
    /* 1) Create one keyboard */
    kb = lv_keyboard_create(parent);
    lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
    lv_obj_set_size(kb, LV_PCT(100), LV_PCT(40));
    lv_keyboard_set_cursor_manage(kb, true);

    /* 2) Create multiple text areas (example: 2; repeat for all 12) */
    lv_obj_t *ta1 = lv_textarea_create(parent);
    lv_obj_set_width(ta1, 200);
    lv_obj_set_pos(ta1, 10, 10);
    lv_obj_add_event_cb(ta1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta1, ta_done_cb,  LV_EVENT_ALL, NULL);

    lv_obj_t *ta2 = lv_textarea_create(parent);
    lv_obj_set_width(ta2, 200);
    lv_obj_set_pos(ta2, 10, 60);
    lv_obj_add_event_cb(ta2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta2, ta_done_cb,  LV_EVENT_ALL, NULL);

    /* ...repeat for ta3..ta12... */



Best Regards,
Zhiming

0 件の賞賛
返信

494件の閲覧回数
sana
Contributor II

Hi 
Thanks for the solution 
I am using lvgl guider 1.9.1 with v9.2.1 selected while creating project.

I did get an error saying there is no reference for 

lv_keyboard_set_cursor_manage

 I have tried my own custom code as you suggested to create input filed text areas but currently i can see overlapping of text area with the keyboard.
how can i overcome this basically i want my page to be scrollable so that user can see through other input check fields by scrolling which will also solve overlapping of keyboard problem i believe.

 

Attaching the screenshot and the code
Please provide me the solution asap

static lv_obj_t *kb;
lv_obj_t *ta_best_load_ratio_val_1;
lv_obj_t *ta_eco_cycle_period_val_1;
lv_obj_t *ta_eco_min_module_no_val_1;
lv_obj_t *ta_rect_save_stop_val_1;
lv_obj_t *ta_dry_time_val_1;
lv_obj_t *ta_best_load_ratio_val_2;
lv_obj_t *ta_eco_cycle_period_val_2;
lv_obj_t *ta_eco_min_module_no_val_2;
lv_obj_t *ta_dcdc_save_stop_val_2;
lv_obj_t *ta_dry_time_val_2;

LV_FONT_DECLARE(lv_font_NotoSans_Regular_18);

/* --- Callbacks --- */
static void ta_focus_cb(lv_event_t *e)
{
    lv_event_code_t code = lv_event_get_code(e);
    lv_obj_t *ta = lv_event_get_target(e);
   

    if(code == LV_EVENT_CLICKED) {
        lv_keyboard_set_textarea(kb, ta);
        lv_obj_clear_flag(kb, LV_OBJ_FLAG_HIDDEN);
         lv_obj_scroll_to_view(ta, LV_ANIM_ON);
    }
}

static void ta_done_cb(lv_event_t *e)
{
    lv_event_code_t code = lv_event_get_code(e);
    lv_obj_t *ta = lv_event_get_target(e);

    if(code == LV_EVENT_READY) {
        const char *val = lv_textarea_get_text(ta);
        /* TODO: commit val to your app logic here */
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
        printf("User entered: %s\n", val);
                fflush(stdout);
        lv_obj_scroll_to_y(lv_obj_get_parent(ta), 0, LV_ANIM_ON);
    } else if(code == LV_EVENT_CANCEL) {
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
    }
}

static void kb_event_cb(lv_event_t * e)
{
    lv_event_code_t code = lv_event_get_code(e);
    lv_obj_t * kb = lv_event_get_target(e);
   
    if(code == LV_EVENT_READY) {
        lv_obj_t * ta = lv_keyboard_get_textarea(kb);
        if(ta) {
            const char * txt = lv_textarea_get_text(ta);
            printf("Committed value: %s\n", txt);
            fflush(stdout);
            // reset bg to default
            lv_obj_set_style_bg_color(ta, lv_color_hex(0xD8D8D8), 0);
            lv_obj_clear_state(ta, LV_STATE_FOCUSED);
            
        }
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
    }
    else if(code == LV_EVENT_CANCEL) {
        lv_obj_t * ta = lv_keyboard_get_textarea(kb);
        if(ta) {
            // reset bg to default
            lv_obj_set_style_bg_color(ta, lv_color_hex(0xD8D8D8), 0);
        }
        lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
        lv_keyboard_set_textarea(kb, NULL);
    }
}


static void textarea_event_cb(lv_event_t * e)
{
    lv_obj_t * ta = lv_event_get_target(e);
    lv_event_code_t code = lv_event_get_code(e);

    if(code == LV_EVENT_CLICKED) {
        // User clicked / focused → mark editable
        lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_EDIT), 0);
    }
    else if(code == LV_EVENT_DEFOCUSED ) {
        // Lost focus (like clicking outside) → reset
        lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_DEFAULT), 0);
    }
}

static void keyboard_event_cb(lv_event_t * e)
{
    lv_obj_t * kb = lv_event_get_target(e);
    lv_event_code_t code = lv_event_get_code(e);

    if(code == LV_EVENT_READY) {   // Tick / OK button pressed
        lv_obj_t * ta = lv_keyboard_get_textarea(kb);
        if(ta) {
            const char * txt = lv_textarea_get_text(ta);

            // Simple validation: check if user entered something
            if(txt && strlen(txt) > 0) {
                printf("User entered: %s", txt);
                fflush(stdout);
            } else {
                printf("No input provided!");
                fflush(stdout);
            }

            // Reset to default once input is taken
            lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_DEFAULT), 0);
        }
    }
}



void screen_init(lv_obj_t *parent)
{
 
   lv_obj_set_scroll_dir(guider_ui.ECO_page, LV_DIR_VER);
   lv_obj_set_scrollbar_mode(guider_ui.ECO_page, LV_SCROLLBAR_MODE_ON);

    /* 1) Create one keyboard */
    kb = lv_keyboard_create(parent);
    lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
    lv_obj_set_size(kb, LV_PCT(100), LV_PCT(40));
    lv_obj_align(kb, LV_ALIGN_BOTTOM_MID, 0, 0);

    // lv_obj_add_event_cb(kb, kb_event_cb, LV_EVENT_ALL, NULL);

    
    ta_best_load_ratio_val_1 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_best_load_ratio_val_1, 279, 132);   
    lv_obj_set_size(ta_best_load_ratio_val_1, 104, 30);  
    lv_obj_set_style_bg_color(ta_best_load_ratio_val_1, lv_color_hex(0xE8E8E8), 0);
    lv_obj_set_style_text_font(ta_best_load_ratio_val_1, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_best_load_ratio_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_best_load_ratio_val_1, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_best_load_ratio_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_best_load_ratio_val_1, LV_OBJ_FLAG_SCROLLABLE);

  
    ta_eco_cycle_period_val_1 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_eco_cycle_period_val_1, 279, 169); 
    lv_obj_set_size(ta_eco_cycle_period_val_1, 104, 30);   
    lv_obj_set_style_bg_color(ta_eco_cycle_period_val_1, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_eco_cycle_period_val_1, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_1, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_eco_cycle_period_val_1, LV_OBJ_FLAG_SCROLLABLE);

    ta_eco_min_module_no_val_1 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_eco_min_module_no_val_1, 693, 95); 
    lv_obj_set_size(ta_eco_min_module_no_val_1, 104, 30);   
    lv_obj_set_style_bg_color(ta_eco_min_module_no_val_1, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_eco_min_module_no_val_1, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_1, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_eco_min_module_no_val_1, LV_OBJ_FLAG_SCROLLABLE);

    ta_rect_save_stop_val_1 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_rect_save_stop_val_1, 693, 132); 
    lv_obj_set_size(ta_rect_save_stop_val_1, 104, 30);   
    lv_obj_set_style_bg_color(ta_rect_save_stop_val_1, lv_color_hex(0xE8E8E8), 0);
    lv_obj_set_style_text_font(ta_rect_save_stop_val_1, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_rect_save_stop_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_rect_save_stop_val_1, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_rect_save_stop_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_rect_save_stop_val_1, LV_OBJ_FLAG_SCROLLABLE);

    ta_dry_time_val_1 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_dry_time_val_1, 693, 169); 
    lv_obj_set_size(ta_dry_time_val_1, 104, 30);   
    lv_obj_set_style_bg_color(ta_dry_time_val_1, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_dry_time_val_1, &lv_font_NotoSans_Regular_18, 0); 
    lv_obj_add_event_cb(ta_dry_time_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dry_time_val_1, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dry_time_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_dry_time_val_1, LV_OBJ_FLAG_SCROLLABLE);

    ta_best_load_ratio_val_2 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_best_load_ratio_val_2, 279, 280);   
    lv_obj_set_size(ta_best_load_ratio_val_2, 104, 30);  
    lv_obj_set_style_bg_color(ta_best_load_ratio_val_2, lv_color_hex(0xE8E8E8), 0);
    lv_obj_set_style_text_font(ta_best_load_ratio_val_2, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_best_load_ratio_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_best_load_ratio_val_2, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_best_load_ratio_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_best_load_ratio_val_2, LV_OBJ_FLAG_SCROLLABLE);

  
    ta_eco_cycle_period_val_2 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_eco_cycle_period_val_2, 279, 317); 
    lv_obj_set_size(ta_eco_cycle_period_val_2, 104, 30);   
    lv_obj_set_style_bg_color(ta_eco_cycle_period_val_2, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_eco_cycle_period_val_2, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_2, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_cycle_period_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_eco_cycle_period_val_2, LV_OBJ_FLAG_SCROLLABLE);

    ta_eco_min_module_no_val_2 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_eco_min_module_no_val_2, 693, 243); 
    lv_obj_set_size(ta_eco_min_module_no_val_2, 104, 30);   
    lv_obj_set_style_bg_color(ta_eco_min_module_no_val_2, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_eco_min_module_no_val_2, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_2, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_eco_min_module_no_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_eco_min_module_no_val_2, LV_OBJ_FLAG_SCROLLABLE);

    ta_dcdc_save_stop_val_2 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_dcdc_save_stop_val_2, 693, 280); 
    lv_obj_set_size(ta_dcdc_save_stop_val_2, 104, 30);   
    lv_obj_set_style_bg_color(ta_dcdc_save_stop_val_2, lv_color_hex(0xE8E8E8), 0);
    lv_obj_set_style_text_font(ta_dcdc_save_stop_val_2, &lv_font_NotoSans_Regular_18, 0);
    lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_dcdc_save_stop_val_2, LV_OBJ_FLAG_SCROLLABLE);

    ta_dry_time_val_2 = lv_textarea_create(parent);
    lv_obj_set_pos(ta_dry_time_val_2, 693, 317); 
    lv_obj_set_size(ta_dry_time_val_2, 104, 30);   
    lv_obj_set_style_bg_color(ta_dry_time_val_2, lv_color_hex(0xD8D8D8), 0);
    lv_obj_set_style_text_font(ta_dry_time_val_2, &lv_font_NotoSans_Regular_18, 0); 
    lv_obj_add_event_cb(ta_dry_time_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dry_time_val_2, ta_done_cb,  LV_EVENT_ALL, NULL);
    lv_obj_add_event_cb(ta_dry_time_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
    // lv_obj_clear_flag(ta_dry_time_val_2, LV_OBJ_FLAG_SCROLLABLE);

    
    // lv_obj_add_event_cb(kb, keyboard_event_cb, LV_EVENT_ALL, NULL);

}


/* Initialize custom UI */
void custom_init(lv_ui *ui)
{
    init_screen_timeout();
    screen_init(ui->ECO_page); 
}

 

タグ(2)
0 件の賞賛
返信

288件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

Please refer the LVGL  manual to use scrolling feature.

https://docs.lvgl.io/master/details/common-widget-features/scrolling.html

Best Regards,
Zhiming

0 件の賞賛
返信