Hi team,
currently i am building screens using lvgl gui guider 1.9.1 for our LCD display
In one of my screens i have used 12 texareas where i need to give user input fields hence multiple keybiards are being used how do i disable those i jus need one keyboard for all the textareas.
Basically user needs to give user inputs for multiple fields for this i am using textareas and clicking on tickmark of keyboard triggers a callback to set this is my use case.
Please provide me the solution ASAP.
Thanks and regards,
sahana
Hi anything on this?
Can the team help me with the faster response.
Thanks and regards,
sahana
Hi,
#include "lvgl.h"
static lv_obj_t *kb;
static void ta_focus_cb(lv_event_t *e)
{
lv_event_code_t code = lv_event_get_code(e);
lv_obj_t *ta = lv_event_get_target(e);
if(code == LV_EVENT_FOCUSED || code == LV_EVENT_CLICKED) {
lv_keyboard_set_textarea(kb, ta);
lv_obj_clear_flag(kb, LV_OBJ_FLAG_HIDDEN);
}
}
static void ta_done_cb(lv_event_t *e)
{
lv_event_code_t code = lv_event_get_code(e);
lv_obj_t *ta = lv_event_get_target(e);
if(code == LV_EVENT_READY) {
const char *val = lv_textarea_get_text(ta);
/* your commit callback here with `val` */
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
} else if(code == LV_EVENT_CANCEL) {
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
}
}
void screen_init(lv_obj_t *parent)
{
/* 1) Create one keyboard */
kb = lv_keyboard_create(parent);
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_obj_set_size(kb, LV_PCT(100), LV_PCT(40));
lv_keyboard_set_cursor_manage(kb, true);
/* 2) Create multiple text areas (example: 2; repeat for all 12) */
lv_obj_t *ta1 = lv_textarea_create(parent);
lv_obj_set_width(ta1, 200);
lv_obj_set_pos(ta1, 10, 10);
lv_obj_add_event_cb(ta1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_t *ta2 = lv_textarea_create(parent);
lv_obj_set_width(ta2, 200);
lv_obj_set_pos(ta2, 10, 60);
lv_obj_add_event_cb(ta2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta2, ta_done_cb, LV_EVENT_ALL, NULL);
/* ...repeat for ta3..ta12... */
Best Regards,
Zhiming
Hi
Thanks for the solution
I am using lvgl guider 1.9.1 with v9.2.1 selected while creating project.
I did get an error saying there is no reference for
lv_keyboard_set_cursor_manage
I have tried my own custom code as you suggested to create input filed text areas but currently i can see overlapping of text area with the keyboard.
how can i overcome this basically i want my page to be scrollable so that user can see through other input check fields by scrolling which will also solve overlapping of keyboard problem i believe.
Attaching the screenshot and the code
Please provide me the solution asap
static lv_obj_t *kb;
lv_obj_t *ta_best_load_ratio_val_1;
lv_obj_t *ta_eco_cycle_period_val_1;
lv_obj_t *ta_eco_min_module_no_val_1;
lv_obj_t *ta_rect_save_stop_val_1;
lv_obj_t *ta_dry_time_val_1;
lv_obj_t *ta_best_load_ratio_val_2;
lv_obj_t *ta_eco_cycle_period_val_2;
lv_obj_t *ta_eco_min_module_no_val_2;
lv_obj_t *ta_dcdc_save_stop_val_2;
lv_obj_t *ta_dry_time_val_2;
LV_FONT_DECLARE(lv_font_NotoSans_Regular_18);
/* --- Callbacks --- */
static void ta_focus_cb(lv_event_t *e)
{
lv_event_code_t code = lv_event_get_code(e);
lv_obj_t *ta = lv_event_get_target(e);
if(code == LV_EVENT_CLICKED) {
lv_keyboard_set_textarea(kb, ta);
lv_obj_clear_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_obj_scroll_to_view(ta, LV_ANIM_ON);
}
}
static void ta_done_cb(lv_event_t *e)
{
lv_event_code_t code = lv_event_get_code(e);
lv_obj_t *ta = lv_event_get_target(e);
if(code == LV_EVENT_READY) {
const char *val = lv_textarea_get_text(ta);
/* TODO: commit val to your app logic here */
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
printf("User entered: %s\n", val);
fflush(stdout);
lv_obj_scroll_to_y(lv_obj_get_parent(ta), 0, LV_ANIM_ON);
} else if(code == LV_EVENT_CANCEL) {
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
}
}
static void kb_event_cb(lv_event_t * e)
{
lv_event_code_t code = lv_event_get_code(e);
lv_obj_t * kb = lv_event_get_target(e);
if(code == LV_EVENT_READY) {
lv_obj_t * ta = lv_keyboard_get_textarea(kb);
if(ta) {
const char * txt = lv_textarea_get_text(ta);
printf("Committed value: %s\n", txt);
fflush(stdout);
// reset bg to default
lv_obj_set_style_bg_color(ta, lv_color_hex(0xD8D8D8), 0);
lv_obj_clear_state(ta, LV_STATE_FOCUSED);
}
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
}
else if(code == LV_EVENT_CANCEL) {
lv_obj_t * ta = lv_keyboard_get_textarea(kb);
if(ta) {
// reset bg to default
lv_obj_set_style_bg_color(ta, lv_color_hex(0xD8D8D8), 0);
}
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_keyboard_set_textarea(kb, NULL);
}
}
static void textarea_event_cb(lv_event_t * e)
{
lv_obj_t * ta = lv_event_get_target(e);
lv_event_code_t code = lv_event_get_code(e);
if(code == LV_EVENT_CLICKED) {
// User clicked / focused → mark editable
lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_EDIT), 0);
}
else if(code == LV_EVENT_DEFOCUSED ) {
// Lost focus (like clicking outside) → reset
lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_DEFAULT), 0);
}
}
static void keyboard_event_cb(lv_event_t * e)
{
lv_obj_t * kb = lv_event_get_target(e);
lv_event_code_t code = lv_event_get_code(e);
if(code == LV_EVENT_READY) { // Tick / OK button pressed
lv_obj_t * ta = lv_keyboard_get_textarea(kb);
if(ta) {
const char * txt = lv_textarea_get_text(ta);
// Simple validation: check if user entered something
if(txt && strlen(txt) > 0) {
printf("User entered: %s", txt);
fflush(stdout);
} else {
printf("No input provided!");
fflush(stdout);
}
// Reset to default once input is taken
lv_obj_set_style_bg_color(ta, lv_color_hex(ECO_LABEL_DEFAULT), 0);
}
}
}
void screen_init(lv_obj_t *parent)
{
lv_obj_set_scroll_dir(guider_ui.ECO_page, LV_DIR_VER);
lv_obj_set_scrollbar_mode(guider_ui.ECO_page, LV_SCROLLBAR_MODE_ON);
/* 1) Create one keyboard */
kb = lv_keyboard_create(parent);
lv_obj_add_flag(kb, LV_OBJ_FLAG_HIDDEN);
lv_obj_set_size(kb, LV_PCT(100), LV_PCT(40));
lv_obj_align(kb, LV_ALIGN_BOTTOM_MID, 0, 0);
// lv_obj_add_event_cb(kb, kb_event_cb, LV_EVENT_ALL, NULL);
ta_best_load_ratio_val_1 = lv_textarea_create(parent);
lv_obj_set_pos(ta_best_load_ratio_val_1, 279, 132);
lv_obj_set_size(ta_best_load_ratio_val_1, 104, 30);
lv_obj_set_style_bg_color(ta_best_load_ratio_val_1, lv_color_hex(0xE8E8E8), 0);
lv_obj_set_style_text_font(ta_best_load_ratio_val_1, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_best_load_ratio_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_best_load_ratio_val_1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_best_load_ratio_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_best_load_ratio_val_1, LV_OBJ_FLAG_SCROLLABLE);
ta_eco_cycle_period_val_1 = lv_textarea_create(parent);
lv_obj_set_pos(ta_eco_cycle_period_val_1, 279, 169);
lv_obj_set_size(ta_eco_cycle_period_val_1, 104, 30);
lv_obj_set_style_bg_color(ta_eco_cycle_period_val_1, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_eco_cycle_period_val_1, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_eco_cycle_period_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_cycle_period_val_1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_cycle_period_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_eco_cycle_period_val_1, LV_OBJ_FLAG_SCROLLABLE);
ta_eco_min_module_no_val_1 = lv_textarea_create(parent);
lv_obj_set_pos(ta_eco_min_module_no_val_1, 693, 95);
lv_obj_set_size(ta_eco_min_module_no_val_1, 104, 30);
lv_obj_set_style_bg_color(ta_eco_min_module_no_val_1, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_eco_min_module_no_val_1, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_eco_min_module_no_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_min_module_no_val_1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_min_module_no_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_eco_min_module_no_val_1, LV_OBJ_FLAG_SCROLLABLE);
ta_rect_save_stop_val_1 = lv_textarea_create(parent);
lv_obj_set_pos(ta_rect_save_stop_val_1, 693, 132);
lv_obj_set_size(ta_rect_save_stop_val_1, 104, 30);
lv_obj_set_style_bg_color(ta_rect_save_stop_val_1, lv_color_hex(0xE8E8E8), 0);
lv_obj_set_style_text_font(ta_rect_save_stop_val_1, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_rect_save_stop_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_rect_save_stop_val_1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_rect_save_stop_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_rect_save_stop_val_1, LV_OBJ_FLAG_SCROLLABLE);
ta_dry_time_val_1 = lv_textarea_create(parent);
lv_obj_set_pos(ta_dry_time_val_1, 693, 169);
lv_obj_set_size(ta_dry_time_val_1, 104, 30);
lv_obj_set_style_bg_color(ta_dry_time_val_1, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_dry_time_val_1, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_dry_time_val_1, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dry_time_val_1, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dry_time_val_1, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_dry_time_val_1, LV_OBJ_FLAG_SCROLLABLE);
ta_best_load_ratio_val_2 = lv_textarea_create(parent);
lv_obj_set_pos(ta_best_load_ratio_val_2, 279, 280);
lv_obj_set_size(ta_best_load_ratio_val_2, 104, 30);
lv_obj_set_style_bg_color(ta_best_load_ratio_val_2, lv_color_hex(0xE8E8E8), 0);
lv_obj_set_style_text_font(ta_best_load_ratio_val_2, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_best_load_ratio_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_best_load_ratio_val_2, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_best_load_ratio_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_best_load_ratio_val_2, LV_OBJ_FLAG_SCROLLABLE);
ta_eco_cycle_period_val_2 = lv_textarea_create(parent);
lv_obj_set_pos(ta_eco_cycle_period_val_2, 279, 317);
lv_obj_set_size(ta_eco_cycle_period_val_2, 104, 30);
lv_obj_set_style_bg_color(ta_eco_cycle_period_val_2, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_eco_cycle_period_val_2, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_eco_cycle_period_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_cycle_period_val_2, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_cycle_period_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_eco_cycle_period_val_2, LV_OBJ_FLAG_SCROLLABLE);
ta_eco_min_module_no_val_2 = lv_textarea_create(parent);
lv_obj_set_pos(ta_eco_min_module_no_val_2, 693, 243);
lv_obj_set_size(ta_eco_min_module_no_val_2, 104, 30);
lv_obj_set_style_bg_color(ta_eco_min_module_no_val_2, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_eco_min_module_no_val_2, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_eco_min_module_no_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_min_module_no_val_2, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_eco_min_module_no_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_eco_min_module_no_val_2, LV_OBJ_FLAG_SCROLLABLE);
ta_dcdc_save_stop_val_2 = lv_textarea_create(parent);
lv_obj_set_pos(ta_dcdc_save_stop_val_2, 693, 280);
lv_obj_set_size(ta_dcdc_save_stop_val_2, 104, 30);
lv_obj_set_style_bg_color(ta_dcdc_save_stop_val_2, lv_color_hex(0xE8E8E8), 0);
lv_obj_set_style_text_font(ta_dcdc_save_stop_val_2, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dcdc_save_stop_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_dcdc_save_stop_val_2, LV_OBJ_FLAG_SCROLLABLE);
ta_dry_time_val_2 = lv_textarea_create(parent);
lv_obj_set_pos(ta_dry_time_val_2, 693, 317);
lv_obj_set_size(ta_dry_time_val_2, 104, 30);
lv_obj_set_style_bg_color(ta_dry_time_val_2, lv_color_hex(0xD8D8D8), 0);
lv_obj_set_style_text_font(ta_dry_time_val_2, &lv_font_NotoSans_Regular_18, 0);
lv_obj_add_event_cb(ta_dry_time_val_2, ta_focus_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dry_time_val_2, ta_done_cb, LV_EVENT_ALL, NULL);
lv_obj_add_event_cb(ta_dry_time_val_2, textarea_event_cb, LV_EVENT_ALL, NULL);
// lv_obj_clear_flag(ta_dry_time_val_2, LV_OBJ_FLAG_SCROLLABLE);
// lv_obj_add_event_cb(kb, keyboard_event_cb, LV_EVENT_ALL, NULL);
}
/* Initialize custom UI */
void custom_init(lv_ui *ui)
{
init_screen_timeout();
screen_init(ui->ECO_page);
}
Hi,
Please refer the LVGL manual to use scrolling feature.
https://docs.lvgl.io/master/details/common-widget-features/scrolling.html
Best Regards,
Zhiming