for MPC5746R,the data transmitted through CAN is available on the message buffers but its not going over the Canlyser. How to check on Canlyser??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

for MPC5746R,the data transmitted through CAN is available on the message buffers but its not going over the Canlyser. How to check on Canlyser??

491 Views
sujendra_n2
Contributor I

microcontroller name: MPC5746R

CAN configuration is done using Eb-Tresos.

2 flexcan with msg ids, One is configured as transmit & other Receive.

While hardware loopback test the data transmitted is available on the message buffers, but is not received on the msg id which was configured as Receive. Canlyser is also not showing Transmitted msg. Please help.

0 Kudos
0 Replies