error in awr - non linear model not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error in awr - non linear model not found

764 Views
hamedradio
Contributor I

Hello my friend

 

I faced some problem using awr modal of some of nxp company transistors, i put the error messaage here to get some help from your side.

3:45:31 PM NXP_AFT05MS031N_Level1_Rev1_SPmodel_FET2.X1 : Element record not found for nonlinear model 'NXP_AFT05MS031N_Level1_Rev1_SPmodel_FET2.X1' component 'FSLRFPK_FET2'

best regards,

Hamed.

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
3 Replies

740 Views
RafaR
NXP Employee
NXP Employee

Hello Hamed

It seems to be a problem with the model kit.

Did you install the high RF power model kit before using the single product model?

Models for Cadence® AWR® Microwave Office® SoftwareOur models are two part :

    RF High power Model Kit
    Product Model Design Kit

Both parts are required to simulate device.

Could you uninstall and install both?, RF High power Model Kit first.

 I've attached a document that will help guide you through the installation. It also has a troubleshooting section that might help you if you suddenly encounter an error.

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 Kudos
Reply

656 Views
hamedradio
Contributor I

Hello, thank you for your response.

I am totally confused really. I downloaded two files for the mentioned transistor.

1)Models for Cadence® AWR® Microwave Office® Software | NXP Semiconductors

version 13- there is no instaling file inside it - so i do not install it and do nothing but unzipping it

2)AFT05MS031N RF High-Power Model AWR Product Model Design Kit.

I downloaded it and followed the following path to have it in awr 

File - new with library - brows and choose the file i got from 2) and  unziped it.

I have the problem i mentioned. 

if it is possible we can set a time to remotely connect to my system and take a look at it please!

Regards,

Hamed

0 Kudos
Reply

572 Views
RafaR
NXP Employee
NXP Employee

Hello hamedradio

Sorry for the delay in responding.

You must download the program directly from AWR. If you have any problems, I recommend contacting their support. AWR support

Then, follow the steps in the PDF I sent you to integrate our libraries.

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 Kudos
Reply