this is my configuration file
Build Configuration:
BB_VERSION = "1.26.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-phytec-linux-gnueabi"
MACHINE = "phyboard-mira-imx6-3"
DISTRO = "yogurt"
DISTRO_VERSION = "i.MX6-PD15.3.0"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):06d9c894636352a6c93711c7284d02b0c794a527"
meta-phytec = "(nobranch):e8166e3e8bf2c26b8665fd52f61890cd851927da"
meta-yogurt = "(nobranch):8f8487fd45b70e7bb68c3ee84463dfb76c72fc2b"
meta-oe
meta-networking
meta-python
meta-multimedia = "(nobranch):a7c1a2b0e6947740758136216e45ca6ca66321fc"
meta-qt5 = "(nobranch):90919b9d86988e7da01fa2c0a07246b5b5600a5d"
meta-ruby = "(nobranch):a7c1a2b0e6947740758136216e45ca6ca66321fc"
the error log is
DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'arm-32', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']
DEBUG: Executing shell function do_install
NOTE: make -j 8 DESTDIR=/home/sajjad/project/build/tmp-glibc/work/cortexa9hf-vfp-neon-phytec-linux-gnueabi/mesa-glut/8.0.0+gitAUTOINC+ee89e9aeb4-r0/image install
make: *** No rule to make target `install'. Stop.
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Function failed: do_install (log file is located at /home/sajjad/project/build/tmp-glibc/work/cortexa9hf-vfp-neon-phytec-linux-gnueabi/mesa-glut/8.0.0+gitAUTOINC+ee89e9aeb4-r0/temp/log.do_install.19493)
if anyone is aware please help
Thanks