difference between TJA1055T/3/1J and TJA1055T/3/1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

difference between TJA1055T/3/1J and TJA1055T/3/1

463件の閲覧回数
佳雯涂
Contributor I

Help!

I do wonder the difference between TJA1055T/3/1J and TJA1055T/3/1

0 件の賞賛
返信
1 返信

460件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

TJA1055T/3/1 - This is the type name for the dual sourced version of the 3V (VIO) version. It can be supplied from either the SSMC wafer fab or from the ICN8 wafer fab.

TJA1055T/3/1J - This is the full orderable part number of the TJA1055T/3/1, the -J indicates that this is the tape and reel packing method.

Best regards,

Tomas

0 件の賞賛
返信