debugger is not connected to pe device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

debugger is not connected to pe device

837 Views
lthomson
Contributor I

I'm trying to debug a k65 microcontroller using code warrior 10.6.4 and a PE Micro programmer and I'm unable to. I can build, and program, start the debugger and the program begins but when it hits a breakpoint or I pause the system, i get the following error:

GDI Protocol Fatal Error

The Debugger is not connected to the PE device

Once this dialog box is closed I then get another that reads:

Runtime error 217 at 0b5227b8

The sequence at the end is unique to that particular execution.

I've tried compatibility modes, reinstalling drivers, other cables, boards, etc. 

Any help would be appreciated. 

0 Kudos
Reply
0 Replies