Hello everyone! We now want to read the UID of 1443B card using clrc663,and also found the driver code RC663_ISO14443B_BeqB.jcf of the development board on the Internet,Now we use the lpc11u68x microcontroller
Serial port to driver clrc663,but we do not know how to configure clrc663 to read the ISO1443B card's UID through
the serial port.Here is some of the driver code:
CLL
CHB 115200
//>Load Protocol
SR 0F 98 // Timer0 Timer starts at the end of transmission
SR 37 FF
SR 14 92 // Timer1 Timber starts at the end of transmission
SR 19 20 // Timer2
SR 1A 03 // TRload Lo
SR 1E 00 // Timer3
SR 02 90 //FIFO control register -> sets FIFO size to 255 bytes
think you!
Hi Wang Ping,
Please kindly refer the attached script for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------