cannot read the data from external memory in mucu like S32R45 etc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

cannot read the data from external memory in mucu like S32R45 etc

1,014 次查看
HyunungPark
Contributor III

I know that the clock is different when HSM works or MCU like the S32R45.

so the function of crypto works normally.

But any data cannot be read from external memory.

what is the solution to resolve this issue?

Hyunung Park

0 项奖励
回复
2 回复数

1,003 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please specify the issue closer?

S32R45 does not have HSM.

But any data cannot be read from external memory.

What data? What configuration? Which SW is used to do so? etc..

Also please state name of company, in case I have to ask internally for help, this is required.

Best regards,

Peter

0 项奖励
回复

976 次查看
HyunungPark
Contributor III

Hi

This issue is resolved.

BRs.

  • Hyunung Park
0 项奖励
回复