cannot read the data from external memory in mucu like S32R45 etc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot read the data from external memory in mucu like S32R45 etc

1,048件の閲覧回数
HyunungPark
Contributor III

I know that the clock is different when HSM works or MCU like the S32R45.

so the function of crypto works normally.

But any data cannot be read from external memory.

what is the solution to resolve this issue?

Hyunung Park

0 件の賞賛
返信
2 返答(返信)

1,037件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please specify the issue closer?

S32R45 does not have HSM.

But any data cannot be read from external memory.

What data? What configuration? Which SW is used to do so? etc..

Also please state name of company, in case I have to ask internally for help, this is required.

Best regards,

Peter

0 件の賞賛
返信

1,010件の閲覧回数
HyunungPark
Contributor III

Hi

This issue is resolved.

BRs.

  • Hyunung Park
0 件の賞賛
返信