can not find swp4 as an inport for LS1028A when testing 802.1CB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not find swp4 as an inport for LS1028A when testing 802.1CB

333 Views
xinliwang
Contributor III

I was tryting to test 802.1CB using LS1028A as a end device. which means swp4 as an inport. and swp0 swp1 swp2 swp3 as outports. 

One typical command is as below:

tsntool> cbgen --device swp0 --index 1 --iport_mask 0x3f --split_mask 0x07 --seq_len 16 --
seq_num 2048

before doing the command i need to build the bridge which i can only attach swp0 ~3 to the bridge and can not find swp4.

 

Tags (1)
0 Kudos
0 Replies