can not find swp4 as an inport for LS1028A when testing 802.1CB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can not find swp4 as an inport for LS1028A when testing 802.1CB

445 次查看
xinliwang
Contributor III

I was tryting to test 802.1CB using LS1028A as a end device. which means swp4 as an inport. and swp0 swp1 swp2 swp3 as outports. 

One typical command is as below:

tsntool> cbgen --device swp0 --index 1 --iport_mask 0x3f --split_mask 0x07 --seq_len 16 --
seq_num 2048

before doing the command i need to build the bridge which i can only attach swp0 ~3 to the bridge and can not find swp4.

 

标记 (1)
0 项奖励
回复
0 回复数