Hi Sir,
Would you help us to check the blhost(2.6.7) error feedback(0x4 & 0x2714)?
What are the error message about 0x4 Invalid Argument Error and 0x2714 (No response packet from target device)?
Solved! Go to Solution.
Hi @StephenYeh
Why are you using the hex 0x0020?, and after the -- flash-erase-all you have a 9, maybe this is giving you an error, are you using an LPC Link 2 to programming? Which MCU are you using? is it a custom board?
Hi Sir
This is the special part, we have fixed this bug. Thanks.
blhost_2.6.7\bin\win>blhost.exe -u 0x1FC9,0x0020 -- get-property 1
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 1258488064 (0x4b030100)
Current Version = K3.1.0
Hi @StephenYeh
Why are you using the hex 0x0020?, and after the -- flash-erase-all you have a 9, maybe this is giving you an error, are you using an LPC Link 2 to programming? Which MCU are you using? is it a custom board?