any one suggest us the Microcontroller which is compiants to IEC61508 standard with lower pin count (less than 100 pins).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

any one suggest us the Microcontroller which is compiants to IEC61508 standard with lower pin count (less than 100 pins).

566件の閲覧回数
arvapallykumara
Contributor I

Hi,

I am Kumaraswamy from Knorr-Bremse,India.We are working into Railway Braking
domain.

In our Project we are designing SIL2 compliant system. In this we require the
Micro controller compliant to IEC 61508 (ISO26262) safety standard with Lower
Pin count(less than 100).

Kindly suggest the same.

0 件の賞賛
返信
0 返答(返信)