about gpio interrupt of lx2160A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about gpio interrupt of lx2160A

755 Views
an897465624
Contributor I

hi, I want to use 4 external-interrupt of GPIO_3 , could I use these port?(GPIO3_13 GPIO3_14 GPIO3_15 GPIO3_16 ) See below. the datasheet only shows dat0~dat11

微信图片_20210918164903.png微信图片_20210918164728.png

 

0 Kudos
2 Replies

743 Views
ufedor
NXP Employee
NXP Employee

> could I use these port?(GPIO3_13 GPIO3_14 GPIO3_15 GPIO3_16 )

These GPIO pins could be used to generate internal interrupt 69 - GPIO3 and GPIO4 ORed.

Refer to the QorIQ LX2160A Reference Manual, 5.2 Internal Interrupt Sources and

20.5.1.4 GPIO interrupt event register (GPIER)

20.5.1.5 GPIO interrupt mask register (GPIMR)

20.5.1.6 GPIO interrupt control register (GPICR)

 

0 Kudos

735 Views
an897465624
Contributor I

Hi,we need these port to be gpio input not out put,for example,such as 1s interrupt input ,10ms interrupt input , 1ms interrupt input ,0.5ms interrupt input  and so on; can we used these ports?

0 Kudos