Where to find source code of AN4772

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to find source code of AN4772

Jump to solution
698 Views
GottiLuca
Contributor IV

On the Freescale Website this application note has been published ( AN4772 , IEC 60730 Safety Routines for the DSC 56800EX Core  ) http://cache.freescale.com/files/32bit/doc/app_note/An4772.pdf?fsrch=1&sr=1

However, I cannot find the source code. There is anyway to get such source code ?

Best Regards,

L.Gotti

0 Kudos
1 Solution
414 Views
pavelrech
NXP Employee
NXP Employee

The safety routines source code is not available to download directly from www.freescale.com as free software. If you want to have the safety routines source code ask appropriate product manager Ron Lowman ( Ron.Lowman@freescale.com ).

Pavel Rech

pavel.rech@freescale.com

View solution in original post

0 Kudos
2 Replies
414 Views
GottiLuca
Contributor IV

Dear Mr. Rech,

Thanks for this precious info.

I'll ask immediately ..

L.Gotti

lgotti@lgl.it

0 Kudos
415 Views
pavelrech
NXP Employee
NXP Employee

The safety routines source code is not available to download directly from www.freescale.com as free software. If you want to have the safety routines source code ask appropriate product manager Ron Lowman ( Ron.Lowman@freescale.com ).

Pavel Rech

pavel.rech@freescale.com

0 Kudos