I would like to know max resolution provided by e-ink display attached with imxebookdc4 e-ink daughter board.
Can i replace the compatible display with smaller or bigger in size? i mean with 6" or 10" or 13"?
Hello Ahesanali Suthar,
The IMXEBOOKDC4 is shipped with panel ED060XH2C1, with a resolution of 1024x758. (I would recommend that you doublecheck the panel that comes with the board. Although I am not aware that there is a different panel on certain boards).
You can change the EPDC on the IMXEBOOKDC4 board to a smaller or bigger EInk panel, just keep in mind that you would need to change the timing structure and the waveform (which must be parsed to work with the i.MX6SL or i.MX7. You may open a Case asking for help parsing the waveform and generating the timing structure.
I hope this helps!
Regards,