What is the default state of SP in CD1020?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the default state of SP in CD1020?

Jump to solution
1,006 Views
jingfang
Contributor IV

What is the default state of SP in CD1020?

Before SP ports and input ports are configured.

0 Kudos
Reply
1 Solution
991 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Before SP ports and input ports are configured, the SP pin is tri-state, and the value of state of  SP depends on the voltage on the SP pin.

The default configure of the SP pin is Switch to Battery (SB). 

If the Voltage is <4V , the state should be  0-open switch.

If the voltage is >4V, the state should be 1-closed switch.

I hope this answers your question.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
3 Replies
992 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Before SP ports and input ports are configured, the SP pin is tri-state, and the value of state of  SP depends on the voltage on the SP pin.

The default configure of the SP pin is Switch to Battery (SB). 

If the Voltage is <4V , the state should be  0-open switch.

If the voltage is >4V, the state should be 1-closed switch.

I hope this answers your question.

Best regards,

Tomas

0 Kudos
Reply
969 Views
jingfang
Contributor IV

Thanks a lot~

How about SG ?

If  Voltage  = 12V, what is the state?

0 Kudos
Reply
964 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

For SG pins, if the voltage is > 4V, the state is open (0). If the voltage is < 4V, the state is closed (1).

Best regards,

Tomas