Hi, All
I have a plan to use a SC18IM700 in my project.
Actually My system was controlled I2C, But now i have to change that to TTL UART signal.
Data sheet for SC18IM700 is show me RS232 transmit & receive input.
My issue is that RS232 UART signals are inverted in polarity with respect TTL UART signal.
My system was controlled TTL level circuit. and, I have a control library already.
So, I don't want to change my library. Then, Do i have to add not-gate for my circuit?
I want to get answer clearly.
Thanks,
Dongsoo
Hi
I don't know much about your system,SC18IM700—an I2C-bus controller with a UART host interface—
is the perfect choice in the case where the host does not have an integrated I2C-bus
controller on-board, and the system designer wishes to use I2C-bus related devices in the
system. Between PC RS232 and SC18IM700 there is also a RS-232 Transceivers.
You can also refer to attached SCH.