Hello,
This is follow up question for this case.
https://community.nxp.com/message/1212814?commentID=1212814&et=watches.email.thread#comment-1212814
a)
I confirmed that TX changed its operation frequency by setting gHAL_bFobActive =1 in power transfer state.
However, this method came to enforce TX to change its operational frequency by FreeMASTER.
I want to check if TX is able to detect a real smart key for car entry and TX change its operational frequency after the detection
What I should do in this case ?
Could you tell me how to evaluate keyfob avoidance function by using the real smart key for car entry in NXP reference board ?
b)
Regarding gHAL_bDBGFobType, there are "level effectively" and "edge effectively".
What is difference between " level effectively " and " edge effectively" ?
How can I evaluate " level effectively " and " edge effectively" in NXP reference board ?
c)
NXP reference board has three coils as TX coil.
I modified the board to use single coil instead of thee coil.
When I installed the program "WCT-15WTXAUTO_V4.0" into the micro controller "MWCT1013AVLH",
TX with single coil was able to charge but could not charge when I installed the program "WCT-15WTXAUTO_V4.1".
Could you tell me how to make TX with single coil work even if I use the program "WCT-15WTXAUTO_V4.1" ?
Thanks,
Norihiro Michigami
AVNET