WCT-15WTXAUTO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WCT-15WTXAUTO

1,262 Views
berniecheah
Contributor I

Hi,

I would like to know the measurement/size of the entire kit. I have searched all user guides and application notes for the measurement but still unable to find it. Are you able to advise on the measurement? Thanks.

Multi-Coil Wireless Charging Transmitter

15W Multi-Coil Automotive Transmitter|NXP 

0 Kudos
3 Replies

1,016 Views
berniecheah
Contributor I

Can i also know the purpose of CAN and IGNITION circuit in the kit?

Is the CAN only for communication interface or is it related with the system flow?

0 Kudos

1,016 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Bernie,

The measurements of the entire kit including connectors, screws and NFC cover are 150mm x 92mm x 25mm.

 

Yes, the CAN interface is for communication between the kit and a car. Unfortunately there is no CAN stack currently available for the kit, only some CAN drivers.

 

The IGNITION signal turns on the power part of the kit. It should be connected to the ignition switch and if you turn it off, the deep sleep mode is activated.

Best regards,

Tomas

 

 

 

 

 

0 Kudos

1,016 Views
berniecheah
Contributor I

Thanks Tomas.

Can I also check with you, where am I able to get the BOM list of this kit?

0 Kudos