Unable to write Port 1 in PCAL6416A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to write Port 1 in PCAL6416A

Jump to solution
1,483 Views
DheerajH
Contributor II

Here we have configured all pins of port 0 as input mode & its working fine but facing issue in output mode of port1.

 

Configured Pin2, Pin3, Pin4, Pin5 & Pin6 of Port1 as output, but unable to set the Pin4 & Pin5 of Port1.

 

The voltage at respective pins are shown in the below table.

 

Port

Voltage observed when pin is set to HIGH(V)

Voltage observed when pin is set to LOW(V)

Port1

Pin2 - 3.3

Pin3 - 3.3

Pin4 - 1.0 (Expected 3.3V)

Pin5 - 1.0 (Expected 3.3V)

Pin6 -  3.3

Pin2 - 0

Pin3 - 0

Pin4 - 1.0 (Expected 0 V)

Pin5 - 1.0 (Expected 0 V)

Pin6 - 0

 attached the Gerber and snap of the schematic in the below link.

https://drive.google.com/drive/u/0/folders/1vk8i7lA49RTkKtkloo1InNvCfmCuyQJ1

Tags (1)
0 Kudos
1 Solution
1,166 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Dheeraj,

 

I see you entered a case #00323999 on this topic three weeks ago. I would recommend you to re-open it so that my colleague Jozef can follow up on this along with our experts from the product group.

 

Best regards,

Tomas 

 

View solution in original post

0 Kudos
7 Replies
1,190 Views
DheerajH
Contributor II

Any updates on this issue?

We have tried with QFN24 Base IC & TSSOP package IC but facing same issue in output mode.

Thank you
Dheeraj

0 Kudos
1,167 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Dheeraj,

 

I see you entered a case #00323999 on this topic three weeks ago. I would recommend you to re-open it so that my colleague Jozef can follow up on this along with our experts from the product group.

 

Best regards,

Tomas 

 

0 Kudos
1,155 Views
DheerajH
Contributor II

 We resolved the issue, there was an issue with I2C protocol

0 Kudos
1,292 Views
DheerajH
Contributor II

Hi Tomas, Thanks for the response...still the same problem exists.

Here we have configured all pins of port 0 as input mode & its working fine but facing issue in output mode of port1.

 

Configured Pin2, Pin3, Pin4, Pin5 & Pin6 of Port1 as output, but unable to set the Pin4 & Pin5 of Port1.

 

The voltage at respective pins are shown in the below table.

 

Port

Voltage observed when pin is set to HIGH(V)

Voltage observed when pin is set to LOW(V)

Port1

Pin2 - 3.3

Pin3 - 3.3

Pin4 - 1.0 (Expected 3.3V)

Pin5 - 1.0 (Expected 3.3V)

Pin6 -  3.3

Pin2 - 0

Pin3 - 0

Pin4 - 1.0 (Expected 0 V)

Pin5 - 1.0 (Expected 0 V)

Pin6 - 0

I have attached the Gerber and snap of the schematic in the below link. Please verify once

https://drive.google.com/drive/u/0/folders/1vk8i7lA49RTkKtkloo1InNvCfmCuyQJ1

0 Kudos
1,473 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Dheeraj,

 

In order to configure Port x for output mode, the following registers should be initialized:

 

Capture_0.JPG

 

Capture_1.JPG

 

Capture_2.JPG

 

Capture_3.JPG

 

Capture_4.JPG

 

So for Port 1, you should configure registers 0x4F, 0x47, 0x49, 0x07 and 0x03. 

 

I hope it helps. If not, please let me know how you set the registers 0x4F, 0x47, 0x49, 0x07 and 0x03 to achieve your required configuration .

 

Best regards,

Tomas

1,466 Views
DheerajH
Contributor II

Thank you Tomas for your response!!

Can you share the values to be configured to make port 1 as output mode with respect to the registers that you have mentioned above.

Below is the configuration that we have done

RegisterValueMode
Configuration Register (06h)0xFFInput Mode
Pullup Enable Register (46h)0xFF 
Pullup Enable Register (47h)0xFF 
   
Configuration Register (07h)0x00Output Mode
Pullup Selection Register (48h)0xFF 
Pullup Selection Register (49h)0xFF 
Output Port Configuration Register (4fh)0x02 

 

Let me know any changes needs to be done in Configuration

Regards,

Dheeraj

0 Kudos
1,459 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Dheeraj,

 

Looking at your configuration, you set all P1 I/Os as open-drain outputs with 100k pull-up resistors. Is this what you want to achieve? 

As I highlighted before, it is recommended to program the register 0x4F before settings the P1 I/Os as outputs. 

Are you now able to set/reset P1 outputs using the the register 0x03? If not, please let me know which outputs do not work and what is connected to them.

 

Best regards,

Tomas

 

0 Kudos