U-Boot Weird Console and DDR Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot Weird Console and DDR Failure

941 Views
Safak28
Contributor II

Hi,

I followed build steps in chapter 3 in "QORIQ-SDK-2.0-IC-REV0.pdf" to create u-boot image for p1020. I used "QorIQ_Linux_SDK_v1.9_PPCE500V2_Yocto_Cache.iso" and "QorIQ_Linux_SDK_v1.9_SOURCE.iso". I used Ubuntu_14.10(Virtual Machine) and/or Ubuntu_16.04(WSL). I didn't got any error message while building. However when i use "u-boot-nor-2015.01+fslgit-r0.bin" to boot my board i got the console. How can i fix this problem?

 

0 Kudos
Reply
4 Replies

717 Views
Safak28
Contributor II

Hi,

I fixed this problem by buiding uboot with buildroot. Thanks for the help.

0 Kudos
Reply

839 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

What is the terminal that you are using? In which platform are you using it?

May you use Tera Term in a Windows host?

Best regards

0 Kudos
Reply

918 Views
Safak28
Contributor II

I have tried different cables with 115200 baud rate

0 Kudos
Reply

927 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

What is the baudrate that your terminal is set to? Also, have you tried using a different cable?

0 Kudos
Reply