The sja1105q dynamic configuration speed is out of order

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The sja1105q dynamic configuration speed is out of order

307 Views
aliang
Contributor I

hello,I use sja1105QS.py, then I change the static configuration of the rate to HOST mode, and the interface of the physical layer is also set to RGMII, then generate configuration groups of C files and write sja1105q, the result is that the PING can be pinged, but iperf3 is used to send UDP packets for testing. sja1105 will cause disorder at 1000M speed. This disorder is very serious, what is the problem? I was hoping you could take a look. Thank you. In addition, if the speed is set to SPEED_1GBPS, as long as it is not HOST,sja1105q will work normally, and there will be no frame loss and out-of-order problems. Would you please look at it for me?

 

aliang_1-1696767264467.png

 

aliang_8-1696767569173.png

aliang_0-1696767156884.png

aliang_2-1696767321510.png

 

0 Replies