TPL sniffing, Saleae Logic, and CRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPL sniffing, Saleae Logic, and CRC?

1,128 Views
BillDuley
Contributor III

Background:

I'm working on the 33772C chip and it seems to be working at the system level with an NXP microcontroller over TPL.

I'm digging deeper and wanting to understand what is being communicated across TPL.

I see that CRC calcs are part of the communication frames and figured this was a great way to establish endianness and confirm I'm understanding bus data correctly.

I can plug the 5 bytes in the 33772C data sheet CRC example in and get the correct CRC with an online calc.

 

My Struggle:

If I plug in data off the bus (via the Saleae logic analyzer) - bad CRC result. 

 

My Question:

Can you advise on what I need to change to make sense of the CRC as viewed with the TPL sniffer?

0 Kudos
Reply
2 Replies

1,089 Views
BillDuley
Contributor III

Got it sorted with the Saleae. Settings in the attached image - maybe it helps someone.

0 Kudos
Reply

1,077 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Bill,

Glad to hear it has already been resolved, thanks for sharing it.

Best regards,

Tomas

0 Kudos
Reply