TJF1052i isolation VDD2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJF1052i isolation VDD2

391件の閲覧回数
Frank8
Contributor I

Question about the TJF1052i


Can you tell me if a continuous voltage of 60 V on VDD2 will affect the output voltage of the pins (VDD1, RxD and TxD) of the microcontroller side despite the isolation?
Do we have to expect the 60V here as well?

I know 60V is ten times the allowed voltage.

0 件の賞賛
返信
3 返答(返信)

372件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Frank,

Could you please share more info about your use case and why do you consider 60V on VDD2 which is indeed rated up to 6V?

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

 

0 件の賞賛
返信

364件の閲覧回数
Frank8
Contributor I

Hello Tomas

We are doing an FMEA right now.
In one of the faults we are looking at, a power supply fails and delivers up to 60V to the VDD2 pin.
We are trying to capture and evaluate all possible faults.
It would be nice to be able to exclude some faults.

 

0 件の賞賛
返信

327件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Frank,

OK, let me check internally whether we have anything else available besides what is in the AH1301, chapter 7 (PIN FMEA).

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

0 件の賞賛
返信