TJF1052i isolation VDD2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJF1052i isolation VDD2

350 Views
Frank8
Contributor I

Question about the TJF1052i


Can you tell me if a continuous voltage of 60 V on VDD2 will affect the output voltage of the pins (VDD1, RxD and TxD) of the microcontroller side despite the isolation?
Do we have to expect the 60V here as well?

I know 60V is ten times the allowed voltage.

0 Kudos
3 Replies

331 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Frank,

Could you please share more info about your use case and why do you consider 60V on VDD2 which is indeed rated up to 6V?

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

 

0 Kudos

323 Views
Frank8
Contributor I

Hello Tomas

We are doing an FMEA right now.
In one of the faults we are looking at, a power supply fails and delivers up to 60V to the VDD2 pin.
We are trying to capture and evaluate all possible faults.
It would be nice to be able to exclude some faults.

 

0 Kudos

286 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Frank,

OK, let me check internally whether we have anything else available besides what is in the AH1301, chapter 7 (PIN FMEA).

Capture.JPG

Capture 1.JPG

Best regards,

Tomas

0 Kudos