TJA1463 CAN FD Bus capacitor value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1463 CAN FD Bus capacitor value

244 Views
saijlr
Contributor I

We are using TJA1463 CAN FD in our design, with a ESD diode which is having 14pF capacitance, how much capacitor need to select for CAN FD purpose, in one of the reference designs I found 37pF.

In TJA1463 Application note AH2002 it is not clear about the capacitor a value, please share the value or calculations to select the CAN FD bus capacitor.

0 Kudos
Reply
3 Replies

224 Views
saijlr
Contributor I

Yes, May I know on which basis they selected 10pF and 27pF capacitor on bus line or how they derived the value for CAN Bus line?

Regards, Sai JLR

 

0 Kudos
Reply

213 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello saijlr,

Once again, thank you for using the NXP community.

Typically, a 10pF to 100pF is used at the connector for ESD.

I hope this information helps.

Regards,

David

0 Kudos
Reply

231 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello saijlr,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I do recommend using the S32G-VNP-RDB2 schematic as a reference for your design.

Do you mean those capacitors?

diazmarin09_0-1714670239859.png

 

I hope this information helps.

Regards,

David

0 Kudos
Reply