TJA1153 pinnig

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1153 pinnig

Jump to solution
278 Views
sametsan88
Contributor I

Hello


TJA1153 is same pinning with TJA1043. Right ? 
If it is not, how can i learn TJA1153 pins ? 

 

Thank you

0 Kudos
Reply
1 Solution
263 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
264 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samet,

Yes, it is the same, except pins #8 (internally connected, should be left floating) and #11 (not connected). You can find the pin configuration in chapter 5 of the TJA1153A datasheet which is classified as a secure file requiring an NDA.

Capture.JPG

Capture 1.JPG

BR, Tomas

0 Kudos
Reply