TJA1145 SPI communication failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1145 SPI communication failure

2,074 Views
空心木头_mm
Contributor I

Hello :

      I am using the can transceiver TJA1145T,and I can not get the right response when I send a 0xfd to it,I am sure I have the right connection among the pins,when I monitored the SDO pin of the TJA1145T,  I found it copy the information I send to it from the pin SDI sometimes,why could this happen ?Can anyone help me?

best regrads!

0 Kudos
Reply
3 Replies

1,529 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Mengmeng,

Do you have an oscilloscope to check if the timing and format of the SPI message is correct? 

A very common problem is that timing parameters are violated, so please make sure everything is in accordance with the following specs:

pastedImage_2.png

pastedImage_3.png

Best regards,

Tomas

0 Kudos
Reply

1,529 Views
1971439734
Contributor II

I have check the format, but i still can't read back the device id, any other solutions? please

0 Kudos
Reply

980 Views
syfchao
Contributor II

hello:

     I have the same problem? do you solve it ?

0 Kudos
Reply