TJA1145局部网络被错误帧(位错误)唤醒

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1145局部网络被错误帧(位错误)唤醒

Jump to solution
9,702 Views
1090097669
Contributor III

TJA145芯片中的局部网络唤醒ID的功能:

    目前存在的疑问是:在芯片休眠之前,配置相应的寄存器中存在问题,使得芯片不仅检测相应的固定IDSignal并且检测Error Frame 并进入计数,超出计数后,错误地唤醒了芯片,使得程序运行异常;

目前休眠的操作步骤是:

1.配置局部网络唤醒的ID和信号;

2.使能局部网络唤醒,使能唤醒事件;

3.清除唤醒事件;

4.进入休眠模式

位错误导致的错误帧会唤醒收发器(不在预期内),继而唤醒芯片。

敢问各位大神,我的操作步骤哪里不对吗?

Labels (2)
Tags (1)
0 Kudos
1 Solution
8,862 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

I attached AN1203 for more detail information about -Application Hints - Partial Networking,please read it before do a wake up function.

View solution in original post

0 Kudos
9 Replies
6,026 Views
Doraemon
Contributor I

你好,我有一个问题,收发器设置选择性唤醒后,可以唤醒芯片,但唤醒后设置成active和normal模式后,运行一段时间后会自动变成offline,且无法进入微控制器接收中断,请问唤醒后的初始化流程有示例吗?

0 Kudos
8,863 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

I attached AN1203 for more detail information about -Application Hints - Partial Networking,please read it before do a wake up function.

0 Kudos
8,862 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please see page12 Software flow: Go to Sleep for more detail!

0 Kudos
8,862 Views
1090097669
Contributor III

I am Sorry ,but,Please Clear ,How to mask the wakeup caused by the error frame?

0 Kudos
8,862 Views
guoweisun
NXP TechSupport
NXP TechSupport

你可能使用了TJA1145,换成TJA1145/FD的版本,把FD-Passive功能打开即可

0 Kudos
8,862 Views
1090097669
Contributor III

我是否可以理解成:TJA1145T这款芯片并不能屏蔽由于位错误帧导致的错误计数器增加,继而唤醒MCU,只有TJA1145FD有这项功能

0 Kudos
8,862 Views
guoweisun
NXP TechSupport
NXP TechSupport

可以这样理解!

8,862 Views
1090097669
Contributor III

Not working at all!

0 Kudos
8,862 Views
1090097669
Contributor III

HI Mr.Sun

   Please point out the corresponding location in this document for my question or give you ideal about this problem,because I have read this document already and could not find the measure of solving  the problem,Thanks.

0 Kudos