TJA1101B PHY Integration to i.MX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA1101B PHY Integration to i.MX8MP

1,470 次查看
Amal_Antony3331
Contributor III

Hi Team,

 We are trying to integrate the NXPs TJA1101 Ethernet PHY with i.MX8MP as a 2-wire interface.
One thing to clarify is that, how can we read/write the MDIO PHY registers?
Are there any utilities available for this ?

Any help is appreciated.

Regards

Amal

标记 (2)
0 项奖励
12 回复数

1,441 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励

1,436 次查看
Amal_Antony3331
Contributor III

 Hi@jimmychan 

I'm able to probe the driver and also set a static IP.

But when I tried to ping to another board which is of same domain, it doesn't work.

So want to read the different status and control register values. So how can we read/write these PHY registers?

 

0 项奖励

1,433 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You could add the code in the driver to read/write the PHY.

0 项奖励

1,413 次查看
Amal_Antony3331
Contributor III

Hi @jimmychan 

I have cross-compiled the attached  application for read the PHY registers.
Register values seems to Okay. but still the communication between tx and rx is not happening.

Link is not getting up. (LINK_STATUS register returns zero).

Whether it is the issue with dts configuration?

0 项奖励

1,398 次查看
jimmychan
NXP TechSupport
NXP TechSupport

What is the configuration of the PHY in your dts file?

0 项奖励

1,395 次查看
Amal_Antony3331
Contributor III

hi @jimmychan 

&fec {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_fec>;
        phy-mode = "rmii";
        phy-handle = <&ethphy1>;
        fsl,magic-packet;
        status = "okay";

        mdio {
                compatible = "fsl,nxp-tja11xx";
                #address-cells = <1>;
                #size-cells = <0>;

                ethphy1: ethernet-phy@0 {
                         compatible = "ethernet-phy-ieee802.3-c22";
                        reg = <0>;
                        eee-broken-1000t;
                        rtl821x,aldps-disable;
                        rtl821x,clkout-disable;
                };
        };
};

        pinctrl_fec: fecgrp {
                fsl,pins = <
                        MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC               0x3
                        MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO              0x3
                        MX8MP_IOMUXC_SAI1_RXD4__ENET1_RGMII_RD0         0x91
                        MX8MP_IOMUXC_SAI1_RXD5__ENET1_RGMII_RD1         0x91
                        MX8MP_IOMUXC_SAI1_TXD7__ENET1_TX_ER             0x1f
                        MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL      0x1f
                        MX8MP_IOMUXC_SAI1_TXD0__ENET1_RGMII_TD0         0x1f
                        MX8MP_IOMUXC_SAI1_TXD1__ENET1_RGMII_TD1         0x1f
                        MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL      0x91
                        MX8MP_IOMUXC_SAI1_TXD6__ENET1_RX_ER             0x1f
                        MX8MP_IOMUXC_SAI1_MCLK__ENET1_TX_CLK            0x3
/*                      MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2         0x91 */
/*                      MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3         0x91 */
/*                      MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC          0x91 */
/*                      MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2         0x1f */
/*                      MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3         0x1f */
/*                      MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC         0x1f */
/*                      MX8MP_IOMUXC_SAI1_RXD0__GPIO4_IO02              0x19 */
                >;
        };
0 项奖励

1,358 次查看
Amal_Antony3331
Contributor III

hi @jimmychan 

Any hint from above?

0 项奖励

1,354 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励

1,338 次查看
Amal_Antony3331
Contributor III

Hi @jimmychan 

How can we read the ENET register values in i.MX8MP.?
 
I tried with memtool , but getting seg error.
 
index.png
 
 
index1.png
How can we read those registers?
 
0 项奖励

1,328 次查看
jimmychan
NXP TechSupport
NXP TechSupport

The base address of ENET in RM is typo.

The base address of fec is 0x30be0000. (you could find the correct address in dts file https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?...)

 

And read an undefined register will result in a bus error. It is better to read the register one by one.

e.g. ./memtool -32 30be0004 1   (read the EIR register)

 

 

0 项奖励

1,449 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 项奖励

1,445 次查看
Amal_Antony3331
Contributor III

Hi @jimmychan 

We are using Linux BSP version : 5.10.35

0 项奖励